cancel
Showing results for 
Search instead for 
Did you mean: 

Include DWARF debug information

gysslypen
Associate
Posted on February 05, 2014 at 09:13

Dear Sir/Madam,

When working with UDE Visual Platform it is possible to view the status of a certain variable. However, in my case it is not possible to view the status of those variables. According to PLS this is due to the fact that no DWARF information is included in the .elf file.

However, SPC5 Studio has defined -ggdb in the common options and this should include DWARF version 2. However, it seems that nothing is included. I am using the compiler ppc-vle-

I am looking forward to your repsonse.

Gijs

----- edit 20140206-------

I have solved the issue
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0