cancel
Showing results for 
Search instead for 
Did you mean: 

Importing existing project in SPC5 studio

Posted on March 16, 2013 at 00:29

I'm trying to import into SPC5 Studio a project before built into Standard Eclipse enviroment but is not clear what should i do.

Should i import it as standard eclipse project or as SPC5 studio project?

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on March 19, 2013 at 12:27

Hi,

From the ''File'' menu select ''Import...'' and then ''General->Existing Projects into Workspace''.

From the dialog select the root of the project(s) and select the ones you want to import.

This procedure is not specific of SPC5Studio, it works in any Eclipse based environment.

Giovanni