2019-04-24 8:07 AM
I have some examples that I acquired through Google searches. There is some trouble right away with trying to init the data flash memory. The ECC will not allow initial writing and gens an IVOR2 fault.
Solved! Go to Solution.
2019-07-19 6:24 AM
Hello James ,
you should install EEPROM Components using the Eclipse Update Site mecanism
(cf screenshot)
Help ==> Install new Software
Update Sites are used to organize and export features so they can be installed into Eclipse applications.
There is a useful help section
Best regards
Erwan
2019-07-18 2:20 AM
Hello ,
We are maintaning SPC560Pxx_RLA EE Test Application for Discovery in SPC5Studio Tools Suite
and SPC560Bxx_RLA ECC Test Application for Discovery
you should mix thiese 2 applications.
Best Regards
Erwan
2019-07-18 9:24 AM
I cannot find a way to access these test applications. Please provide further explanation to gain access.
Thanks
2019-07-19 6:06 AM
Please install SPC5Studio Tools Suite
https://www.st.com/en/development-tools/spc5-studio.html
and install them from http://download.spc5studio.com/
The address component location are in this web address
Best Regards
Erwan
2019-07-19 6:12 AM
I have already installed SPC5Studio. I am puzzled by where to navigate to inside the tool to find the two articles you named. Again, please provide further detail on where to access them.
2019-07-19 6:24 AM
Hello James ,
you should install EEPROM Components using the Eclipse Update Site mecanism
(cf screenshot)
Help ==> Install new Software
Update Sites are used to organize and export features so they can be installed into Eclipse applications.
There is a useful help section
Best regards
Erwan