2021-05-03 7:12 AM
Hi,
I am using SPC584b60e MCU, I have to write several hundred byte of data at Customer OTP region which is there in first block flash memory. I am not getting how I can start. I have following question
1) Can I use C55 flash module API to write at this region, if so how I can start, because I don't see any example for writing at OTP region in SPC5 studio ?
2) Can I write data here word by word (32-bit at a time ) instead of whole block write ?
3) What is sequence to initialize, unlock and write at this customer OTP location.
Please provide if any example code is available
Thank you
Solved! Go to Solution.
2021-06-02 6:39 AM
Hello Nundi ,
you can use C55 flash module API in order to write in One-Time Programmable (OTP) area Test Flash Block
for thers questions, i recommend to go in the RM0449 for additional questions.
Best Regards
Erwan
2021-06-02 6:39 AM
Hello Nundi ,
you can use C55 flash module API in order to write in One-Time Programmable (OTP) area Test Flash Block
for thers questions, i recommend to go in the RM0449 for additional questions.
Best Regards
Erwan