2019-07-01 4:19 AM
.i need help with calculating clock and time peroid and waht is other pwm pin if pwm0 has d10 which is complemetary pin in spc56el70l5-disp
Solved! Go to Solution.
2019-07-25 11:27 PM
i tried to cut down reset circuit issue is core is giving ground..
lvcor is fine with 1.2v constant..
par number is spc56el60l5ccosr
2019-07-25 11:32 PM
2019-07-25 11:48 PM
core inactive no lockstep mode is detected message from debugger
2019-07-25 11:54 PM
Hi,
so, summarizing, if you cut the external reset circuit, unplug the debugger, power the board and monitor the pin RESET_B, this pin is always low. Right?
Regards,
Luigi
2019-07-25 11:57 PM
2019-07-26 12:01 AM
Please, could you confirm that if you cut the external reset circuit, unplug the debugger, power the board, the pin RESET_B is always low?
Regards,
Luigi
2019-07-26 12:21 AM
yes you are absolutely right..thats the issue..
2019-07-26 12:28 AM
i cut the external reset circuit, unplugged the debugger, power the board, the pin RESET_B is always giving low..that is main problem..in discovery it is not it works well...for my circuit is gives low ..always
2019-07-26 12:39 AM
i have developed four pcb board with four differnt ic ...all got same issue..cheked power supply and reset circuit...but reset is low while i power up...i dont know what to do next..help out..
2019-07-26 1:54 AM