2018-09-18 05:41 PM
When I import example projects for my SPC58 board, I am able to edit the I/O settings. Specifically, I can change the I/O mode of GPIO pins to be input or output instead of both, which I can't do from the Pin Map editor.
But when I try and select this component on my own project, the I/O settings are disabled. I can see the configurations I've made in the Pin Map editor, but I can't change anything.
Does anyone know how to enable this? I'm using SPC5 Studio 5.8
Thanks,
2018-09-19 01:27 AM
Hello ,
Could you give me the family name (which SPC58) ?
Best regards
Erwan