2019-11-12 10:37 PM
I am using Init package component (in which irq, osal, etc. components are present). When I use just timer interrupt, it gets successfully run. however, when I am trying to add UART peripheral inside the code, it gets stuck at _IVOR1. What can be the reason of this behaviour?
Also, inside OSAL component, Timer 0 is configured, can anyone please elaborate the use of Timer 0 over there?
Solved! Go to Solution.
2019-11-13 5:51 AM
Hello ,
There are some examples in the test applications in SPC5Studio.
by the debugger you can rebuild the stack and check where the problem occured before the IVOR1
Best Regards
Erwan
2019-11-13 5:51 AM
Hello ,
There are some examples in the test applications in SPC5Studio.
by the debugger you can rebuild the stack and check where the problem occured before the IVOR1
Best Regards
Erwan