2020-10-08 01:10 AM
I recognized that a lot of components are incompatible with my SPC574S-DISP-Board. Why? It looks like its available on the K-Version.
Solved! Go to Solution.
2020-10-13 02:21 AM
Hello ,
According to the RM, GTM is not present in SPC574S-DISP Board. (RM0349)
Best Regards
Erwan
2020-10-13 02:21 AM
Hello ,
According to the RM, GTM is not present in SPC574S-DISP Board. (RM0349)
Best Regards
Erwan
2020-10-16 02:30 AM
Hi,
are there any alternatives to this component? Or is it possible to get an example how to generate the pwm signal overwise?
Best regards,
Niklas
2020-11-02 04:33 AM
Hello,
use the FlexPWM instead.
In SPC5Studio, select the SPC574S (SPHAERO) device and do not select the board, a PWM test aplication is then available,
Even if not specifically written for SPC570S-DISP board, this application works also for DISP board.
Regards,
Giuseppe