cancel
Showing results for 
Search instead for 
Did you mean: 

GTM component for SPC574S?

NDorn.1
Associate II

I recognized that a lot of components are incompatible with my SPC574S-DISP-Board. Why? It looks like its available on the K-Version.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello ,

According to the RM, GTM is not present in SPC574S-DISP Board. (RM0349)

Best Regards

Erwan

View solution in original post

3 REPLIES 3
Erwan YVIN
ST Employee

Hello ,

According to the RM, GTM is not present in SPC574S-DISP Board. (RM0349)

Best Regards

Erwan

Hi,

are there any alternatives to this component? Or is it possible to get an example how to generate the pwm signal overwise?

Best regards,

Niklas

Giuseppe DI-GIORE
ST Employee

Hello,

use the FlexPWM instead.

In SPC5Studio, select the SPC574S (SPHAERO) device and do not select the board, a PWM test aplication is then available,

Even if not specifically written for SPC570S-DISP board, this application works also for DISP board.

Regards,

Giuseppe