cancel
Showing results for 
Search instead for 
Did you mean: 

Green Hills Compiler Support SPC5 Studio

NMazz.2
Associate II

I am attempting to get the GHS compilier to build with SPC58NG dev kit and have switched the Build settings to below

 0693W00000BcE2fQAF.pngI have updated the project to include the path and commented out the error statement

ifeq ($(GHS_PATH),)

export PATH := C:\ghs\comp_202114\$(PATH_SEPARATOR)${PATH}

 # $(error Please specify a valid path into GHS_PATH for ccppc (GHS) compiler)

endif

and it will compile but then include some strange error that doesn't really help. Is there any setting I need to fix it looks to be something in the linking process.

0693W00000BcE2kQAF.png

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

TBH this looks circular, adding to the PATH for executables / tools

export PATH := C:\ghs\comp_202114\$(PATH_SEPARATOR)${PATH}

Surely you want to be exporting GHS_PATH, not PATH, as presumable used elsewhere in the scripting or INCLUDE / LIB paths, etc. Or that GHS_PATH exists from the outset in your installed environment.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

4 REPLIES 4

>>compile but then include some strange error that doesn't really help

Says the linker failed because it can't find a symbol/function to bind with.

Either you're missing a source, or object file, or you have some #ifdef level exclusion of code you actually need, but isn't supplied for the GHS tools.

Perhaps start by figuring out what symbol it is choking on, a partial .MAP or linker output? Increase verbosity level if appropriate.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
NMazz.2
Associate II

Yeah okay it was missing a callback that didnt bother gcc.

On another note every time I regenerate something, the makefile gets regenerated and I have to rewrite the fix in the makefile.

I have added ghs to my path variables on my machine and also in the project. Any work arounds for this?

ifeq ($(GHS_PATH),)

 $(error Please specify a valid path into GHS_PATH for ccppc (GHS) compiler)

endif

TBH this looks circular, adding to the PATH for executables / tools

export PATH := C:\ghs\comp_202114\$(PATH_SEPARATOR)${PATH}

Surely you want to be exporting GHS_PATH, not PATH, as presumable used elsewhere in the scripting or INCLUDE / LIB paths, etc. Or that GHS_PATH exists from the outset in your installed environment.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Erwan YVIN
ST Employee

Yes , it is in Windows Preferences , you should add the GHS_PATH in your environment ;)