2018-05-22 4:47 AM
HI,
I found an FCCU exception while running some code in Stop mode in SPC58NE84C3(6M). The source for the FCCU is from MEMU(MEMU_RAM_UCE_22) but i do not know why this error is occurring. Since i'm using Isystem IC5500 debugger which doesn't support low power debugging for 6M variant in my case. Please have a look at attached SFR info and let me know if further info. is needed.
#fccu #automotive-microcontrollers #spc58 #memuSolved! Go to Solution.
2018-05-25 6:25 AM
Hello Manjunatha,
Sorry, I have not the right to discuss 58 family on this forum.
Please contact :
https://my.st.com/content/my_st_com/en/support/support-home.html
Best regards
Erwan
2018-05-23 1:13 AM
Hello ,
28
SR_UCESystem RAM ECC and MBIST Uncorrectable Error Detect flag.Asserted when:– A new System RAM ECC and MBIST uncorrectable error is detected– A new entry to the uncorrectable error reporting table is done (either by CPU ormodule)0 No new and unique error detected.1 New entry in uncorrectable error reporting table is made.This error can not be corrected from FCCU.
it seems to be relative to the STOP mode
I have requested some help from some experts.
Best regards
Erwan
2018-05-23 3:45 AM
Hello ,
we have missed in your log :
SYS_RAM_UNCERR_ADDR = 010B7AC8
ERR_ADD = 010B7AC8
0x01000000 0x01FFFFFF 16 MB 5888 KB Large Flash Blocks �? no overlay
it seems to be a bad fetch in your program.
did you stop the flash in the STOP mode ?
Best regards
Erwan
2018-05-25 6:25 AM
Hello Manjunatha,
Sorry, I have not the right to discuss 58 family on this forum.
Please contact :
https://my.st.com/content/my_st_com/en/support/support-home.html
Best regards
Erwan
2018-05-25 7:14 AM
Hi
Erwan,
Thanks for the response.
well
a const structure variable is stored in 0x
010B7AC8.
I did not stop the flash in stop mode. In fact i don't even know whether it is enabled or stopped in stop mode, please let me know is there any way to check it.
Is flash wait state affects the bad fetch?
Thank you,
Manjunatha