cancel
Showing results for 
Search instead for 
Did you mean: 
This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
5 REPLIES 5
Erwan YVIN
ST Employee
Posted on May 03, 2016 at 17:12

Hello Cal ,

the marketplace is working well.

did you use a proxy or a firewall ?

Often ,the firewall can lock the marketplace.

you can try to use directly the update site

Help ==> Install New Software

  Best regards

                 Erwan

alberto2399
Associate II
Posted on May 04, 2016 at 11:43

Thank you Erwan!

Could you indicate the update site?

Cel

Erwan YVIN
ST Employee
Posted on May 04, 2016 at 13:50

Hello cel ,

The update site is 

http://spc5.drive.cloudforge.com/projects/spc5releases/SPC5Studio/updates4/

Normally , it is stored in SPC5Studio configuration

  Best regards

             Erwan

alberto2399
Associate II
Posted on May 04, 2016 at 14:54

I was able to download the compiler. I guess that now I should configure the compiler through the ''external tool configuration''. 

I probably need the location and the arguments of the compiler and maybe other settings. Could you provide me this information?

Thanks again,

Cel

Erwan YVIN
ST Employee
Posted on May 13, 2016 at 11:29

Hello Cel ,

When you are switching into ppc-freevle-eabi-

the options are automatically set.

The compiler update is based on a standard gcc distribution with VLE support.

You can find gcc 4.9.3 documentation here:

Best regards

Erwan

________________

Attachments :

2016-05-13_112726.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qVg1&d=%2Fa%2F0X0000000bnz%2Fru8T2lCRkB4J1rCCXRN6rQJXgQuW8L.9hY9i.XQZwhQ&asPdf=false