2016-05-03 3:24 AM
Hello everybody,
I've installed SPC5Studio and, following the indication, I've tried to install the compiler from Eclipse Marketplace, but I've received the following error message:''MarketplaceDiscoveryStrategy failed with an errorCannot complete request to http://vps182808.ovh.net:9090/marketplace/api/p?product=com.st.tools.spc5.studio.spc5Studio&platform.version=4.4.2.v20150204-1700&os=win32&java.version=1.8.0_45&client=org.eclipse.epp.mpc.core&product.version=3.0.0.201512011640&runtime.version=3.10.0.v20140318-2214&ws=win32&nl=it_IT: Unable to read repository at http://vps182808.ovh.net:9090/marketplace/api/p?product=com.st.tools.spc5.studio.spc5Studio&platform.version=4.4.2.v20150204-1700&os=win32&java.version=1.8.0_45&client=org.eclipse.epp.mpc.core&product.version=3.0.0.201512011640&runtime.version=3.10.0.v20140318-2214&ws=win32&nl=it_IT.Unable to read repository at http://vps182808.ovh.net:9090/marketplace/api/p?product=com.st.tools.spc5.studio.spc5Studio&platform.version=4.4.2.v20150204-1700&os=win32&java.version=1.8.0_45&client=org.eclipse.epp.mpc.core&product.version=3.0.0.201512011640&runtime.version=3.10.0.v20140318-2214&ws=win32&nl=it_IT.vps182808.ovh.net:9090 failed to respond''Could you kindly help me?Thanks!2016-05-03 8:12 AM
2016-05-04 2:43 AM
Thank you Erwan!
Could you indicate the update site?Cel2016-05-04 4:50 AM
http://spc5.drive.cloudforge.com/projects/spc5releases/SPC5Studio/updates4/
Normally , it is stored in SPC5Studio configuration Best regards Erwan2016-05-04 5:54 AM
I was able to download the compiler. I guess that now I should configure the compiler through the ''external tool configuration''.
I probably need the location and the arguments of the compiler and maybe other settings. Could you provide me this information?Thanks again,Cel2016-05-13 2:29 AM
Hello Cel ,
When you are switching into ppc-freevle-eabi- the options are automatically set. The compiler update is based on a standard gcc distribution with VLE support. You can find gcc 4.9.3 documentation here: Best regards Erwan ________________ Attachments : 2016-05-13_112726.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qVg1&d=%2Fa%2F0X0000000bnz%2Fru8T2lCRkB4J1rCCXRN6rQJXgQuW8L.9hY9i.XQZwhQ&asPdf=false