2018-06-29 06:41 AM
Dear All ,
Runtime IO Component is available for SPC5Studio 5.8.0.
What is Runtime IO Component?
The Runtime IO Component allow you to use the standard printf function to write an output message. As first implementation the stdout is redirect, throgh the freopen, to the serial device, in the future (when the support will be added) it can be redirect on CAN or Ethernet device. So to correctly initialize the serial driver, it needs to configure the Runtime IO component selecting the properly device to use, depending which platform we are using.
to install this component ,
you have to use this update site in Help ==> install new software
http://download.spc5studio.com/updates/
Best regards
Erwan
#spc5 #spc5studio