2025-11-13 11:12 AM - last edited on 2025-11-13 11:40 AM by Peter BENSCH
Hi everyone,
I’m working on configuring the SARADC in the SPC58ECxx using the RLA (Low-Level Drivers) tool. I want to read an analog signal on PE0 / ADC-AN11.
In the SARADC settings, I see the following options:
SARADC B
SARADC 0
SARADC 1
SARADC 3
SARADC 10bit modules
SARADC STANDBY
I’m a bit confused about which options I actually need to select. I understand that SARADC0 is the module connected to my pin, but I’m not entirely clear on the purpose of SARADC B and the other options.
Could someone clarify:
What each of these options actually does.
Which options I need to select if I only want to read PE0 / AN11 with SARADC0.