cancel
Showing results for 
Search instead for 
Did you mean: 

Command line operations with the SPC5Studio

GKove
Associate

Hi,

With SPC5Studio 5.8.1, is there a command line option to generate the SPC5 application? Or a headless way to generate and build the project?

I'm looking into non-GUI interactions with the environment so that generation and building can be scripted.

I'll appreciate any information about this.

Best regards,

Gregory

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello Gregory ,

It is a good question

I think that you can use RCPTT or a project like

https://code.google.com/archive/p/headlesseclipse/

I am looking an Alternative for your problematic

Best Regards

Erwan

View solution in original post

4 REPLIES 4
Erwan YVIN
ST Employee

Hello Gregory ,

It is a good question

I think that you can use RCPTT or a project like

https://code.google.com/archive/p/headlesseclipse/

I am looking an Alternative for your problematic

Best Regards

Erwan

madanAde
Associate

Hi Gregory,

I am also looking for non-GUI compilation for SPC studio project, Have you successful with the command line setup? I appreciate if you can share any more information, thanks

I didn't find any way to generate the project files using CLI, but once it's generated, I could work with the generated makefiles and sources.

NMazz.1
Associate II

I found placing this in a batch file gets it to work

C:/SPC5Studio/eclipse/SPC5Studio.exe --launcher.suppressErrors -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "c:\spc5_headlessBuilds" -import "%cd%" -build *