2023-03-17 2:19 AM
Solved! Go to Solution.
2023-03-20 1:09 AM
As mentioned, the H stands for an internal information from the production of the device that has no influence on the behaviour of the STB37N60DM2AG and is therefore irrelevant for the user.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter
2023-03-17 3:14 AM
Welcome, @CPerf.1, to the community!
Since you have not uploaded a photo of the components in question, one can only assume that this is internal additional information that is included with some D2PAK.
Regards
/Peter
2023-03-19 11:14 PM
2023-03-20 1:09 AM
As mentioned, the H stands for an internal information from the production of the device that has no influence on the behaviour of the STB37N60DM2AG and is therefore irrelevant for the user.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter