cancel
Showing results for 
Search instead for 
Did you mean: 

AEK-POW-BMS63EN Short CIrcuit on Daisy Chain

Vipuls
Associate II

Hello Community,

I have an observation from my attempt to daisy chain multiple AEK-POW-BMS63EN devices. 

I have made a battery pack which has two 14-cell Battery modules in series. One module is supposed to be connected to one AEK-POW-BMS63EN and send data over ISOSPI lines back to the AEK-ISOSPI-SPI Translator and then to the master, which is AEK-MCU-C4MLIT1. 

I validated the individual slaves first, and they were working. However, when I connected the ISOH line of my first slave with the ISOL line of the second slave, it created a short circuit, and the slave IC burnt. I want to know what the correct configuration is for connecting the ISOSPI lines for a daisy chain. 

I have attached my configuration in the attached photo. 

Thank you

Regards,

Vipul

0 REPLIES 0