2022-09-30 4:29 AM
i have set enables 1,2,3 and 4 as 1100 which is address 2 , but for some reason the speaker is not open and voltage is not passing through it which means i cant move on and give orders through i2c registers, can you please explain what the reason might be?
Solved! Go to Solution.
2022-10-03 8:15 AM
For point 3. please refer to paragraph 8.1 of User Manual UM2623
or watch the following YouTube self learning video 1
https://www.youtube.com/watch?v=WDp4XmmwEwc&list=PLnMKNibPkDnEju3j_qhe-MFK-NnwD_kuP
If you watch all 8 videos of 10min each it will give you a basic understanding of
how the environment works.
Regards,
AutoDevKit Team
2022-09-30 8:11 AM
Dear Sir,
As you can understand, it is not possible for us to help you debug the NXP microcontroller. I can only report the init procedure we use. For the configuration of the MCU peripherals you should consult with NXP.
The Init() function for the FDA903D is the following (on our Microcontroller):
// The following line reset the address signals
pal_lld_clearpad(Enables_ARRAY[dev][0], Enables_ARRAY[dev][1]);
pal_lld_clearpad(Enables_ARRAY[dev][2], Enables_ARRAY[dev][3]);
pal_lld_clearpad(Enables_ARRAY[dev][4], Enables_ARRAY[dev][5]);
pal_lld_clearpad(Enables_ARRAY[dev][6], Enables_ARRAY[dev][7]);
// We wait a period to stabilize the signals
osalThreadDelayMilliseconds(500);
//Enables address with combination 1100 0xE2
pal_lld_setpad(Enables_ARRAY[dev][0], Enables_ARRAY[dev][1]); //Enable 1 = 1
pal_lld_setpad(Enables_ARRAY[dev][2], Enables_ARRAY[dev][3]); //Enable 2 = 1
pal_lld_clearpad(Enables_ARRAY[dev][4], Enables_ARRAY[dev][5]); //Enable 3 = 0
pal_lld_clearpad(Enables_ARRAY[dev][6], Enables_ARRAY[dev][7]); //Enable 4 = 0
// Initialize register with default value
uint8_t data[15];
// Init: Turn IB registers into application default setting
data[0] = IB0_DEFAULT; // data[0] = 0x00;
data[1] = IB1_DEFAULT; // data[1] = 0x00;
data[2] = IB2_DEFAULT; // data[2] = 0x00;
data[3] = IB3_DEFAULT; // data[3] = 0x38;
data[4] = IB4_DEFAULT; // data[4] = 0x00;
data[5] = IB5_DEFAULT; // data[5] = 0x00;
data[6] = IB6_DEFAULT; // data[6] = 0x00;
data[7] = IB7_DEFAULT; // data[7] = 0x00;
data[8] = IB8_DEFAULT; // data[8] = 0xC0;
data[9] = IB9_DEFAULT; // data[9] = 0x00;
data[10] = IB10_DEFAULT; // data[10] = 0x50;
data[11] = IB11_DEFAULT; // data[11] = 0x30;
data[12] = IB12_DEFAULT; // data[12] = 0x00;
data[13] = IB13_DEFAULT; // data[13] = 0x20;
data[14] = IB14_DEFAULT; // data[14] = 0x09;
AEK_903D_Write_IB(dev, IB0, &data[0], 15); // IB14[0] = 1; FIRST bit
The function to send the first message is:
i2c_result_t AEK_903D_Write_IB(AEK_AUD_D903V1_DEVICE dev, uint8_t reg_addr, uint8_t * data, uint8_t size)
{
// Check address range
if (reg_addr > FDA903D_IB_ADDR_MAX)
{
return I2C_ERROR_INVALID_ADDRESS;
}
if (size > 1)
{
reg_addr |= 0x80; // Continues Write
}
return i2c_lld_write(AEK_AUD_D903V1_I2C_ARRAY_DRIVER[dev],(uint8_t)I2CAddress[dev], reg_addr, data, size);
}
I hope it helps!
Best Regards,
AutoDevKit Team
2022-09-30 8:14 AM
The full code for our microcontroller SPC582B is available on AutoDevKit www.st.com/autodevkitsw
2022-10-03 4:15 AM
Mr. Max , if i give my enables 1100 without doing any other procedure, the speaker should open right?
Also , do i need to reset the values of the enables and registers to 0?
2022-10-03 4:22 AM
The Enables set the I2C address nothing to do with the speaker.
Please follow the entire procedure include register reset to activate the I2C.
2022-10-03 4:33 AM
im trying to understand the code, so after setting the enables we have to reset the register values as you specified, and then write messages to them according to our command. thats right?
2022-10-03 4:51 AM
Mr max
also can u explain the procedure to open the speaker ?
2022-10-03 5:27 AM
you need to follow the state machine to reach mute and play states and send I2S data
Please refer page 28 of FDA903D datasheet
FDA903D - 1 x 45 W class D digital input automotive power amplifier
Here is the User Manual
2022-10-03 5:57 AM
ok how can i open the example code you provided, i have downloaded the library and installed it.
or can you just give the full code here please.
2022-10-03 8:15 AM
For point 3. please refer to paragraph 8.1 of User Manual UM2623
or watch the following YouTube self learning video 1
https://www.youtube.com/watch?v=WDp4XmmwEwc&list=PLnMKNibPkDnEju3j_qhe-MFK-NnwD_kuP
If you watch all 8 videos of 10min each it will give you a basic understanding of
how the environment works.
Regards,
AutoDevKit Team