2022-09-30 4:29 AM
i have set enables 1,2,3 and 4 as 1100 which is address 2 , but for some reason the speaker is not open and voltage is not passing through it which means i cant move on and give orders through i2c registers, can you please explain what the reason might be?
Solved! Go to Solution.
2022-10-06 5:08 AM
Mr max, im trying to follow the I2C register reset, but when i want to send some data to an address (for example address register 8) it gives me on my logic analyzer 0B0001000 + NACK, so i cant send data without the ack bit. do you know what could be possibly the mistake?
2022-10-06 6:39 AM
Dear Sir,
It is not easy to help you debug the communication of a microcontroller I do not know.
I can only try to give two general suggestions:
Finally, you should already have the source code in AutoDevKit, therefore you can copy from there how to properly prepare the i2C packet.
2022-10-07 4:49 AM
ok Mr max thanks for the support, do you have demo like the one you have sent that works on stm32f429i Discovery card?
2022-10-07 5:31 AM
Dear Sir,
The demo is written for SPC58 microcontrollers.
You are free to port it on STM32 if needed.
Regards,
AutoDevKit Team
2022-10-07 5:33 AM
Mr max, i have decided to use STM32F429ZI MCU from the f429 discovery card, do you have any demos that works with the FDA903D if not can you show me example codes so i can use it and built my own code? thank you
2022-10-07 5:38 AM
İ have to install the library on stm32 right?
2022-10-07 6:31 AM
Just take the driver of FDA903 from SPC58 and change the low-level calls to STM32. Just be careful that SPC58 is big endian while STM32 is little endian.
2022-10-10 5:33 AM
Mr max , i took the driver and inclluded it to my project, the code i wrote is like this:
my functions:
void AEK_903D_Init()
{
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_8, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_10, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_14, GPIO_PIN_RESET);
HAL_Delay(500);
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_8, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_10, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_14, GPIO_PIN_RESET); // I2C adress is 0100 = 0xE0
}
uint16_t AEK_903D_SetDefaultRegisters()
{
HAL_StatusTypeDef status;
uint8_t data[15];
uint8_t play = 0B11100001;
// Init: Turn IB registers into application default setting
data[0] = IB0_DEFAULT; // data[0] = 0x00;
data[1] = IB1_DEFAULT; // data[1] = 0x00;
data[2] = IB2_DEFAULT; // data[2] = 0x00;
data[3] = IB3_DEFAULT; // data[3] = 0x38;
data[4] = IB4_DEFAULT; // data[4] = 0x00;
data[5] = IB5_DEFAULT; // data[5] = 0x00;
data[6] = IB6_DEFAULT; // data[6] = 0x00;
data[7] = IB7_DEFAULT; // data[7] = 0x00;
data[8] = IB8_DEFAULT; // data[8] = 0xC0;
data[9] = IB9_DEFAULT; // data[9] = 0x00;
data[10] = IB10_DEFAULT; // data[10] = 0x50;
data[11] = IB11_DEFAULT; // data[11] = 0x30;
data[12] = IB12_DEFAULT; // data[12] = 0x00;
data[13] = IB13_DEFAULT; // data[13] = 0x20;
data[14] = IB14_DEFAULT; // data[14] = 0x09;
//return AEK_903D_Write_IB(dev, IB0, &data[0], 15); // IB14[0] = 1; FIRST bit
status = HAL_I2C_Mem_Write(&hi2c1, 0xE0, IB8, 15, &play, 15, 100); // play is 11100001 which puts PWM on and plays
if(HAL_OK == status)
{
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_13, GPIO_PIN_SET);
return 1;
}
return 0;
}
in my main:
int main(void)
{
/* USER CODE BEGIN 1 */
//findF_Out(1250);
sample_dt = F_OUT/F_SAMPLE;
sample_N = F_SAMPLE/F_OUT;
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_I2C1_Init();
MX_I2S3_Init();
MX_CAN1_Init();
/* USER CODE BEGIN 2 */
if( HAL_CAN_Start(&hcan1) != HAL_OK)
{
Error_Handler();
}
// CAN notification
if(HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
{
Error_Handler();
}
sample_dt = F_OUT/F_SAMPLE;
sample_N = F_SAMPLE/F_OUT;
AEK_903D_Init();
AEK_903D_SetDefaultRegisters();
for(uint16_t i=0; i<sample_N; i++){
mySinVal = sinf(i*2*PI*sample_dt);
dataI2S[i*2]=(mySinVal+0)*8000;
dataI2S[i*2+1]=(mySinVal+0)*8000;
}
HAL_I2S_Transmit_DMA(&hi2s3, (uint16_t *)dataI2S, sample_N*2);
HAL_DAC_Start(&hdac, DAC1_CHANNEL_1);
HAL_TIM_Base_Start_IT(&htim2);
QUESTION 1: is the function that sends play correct?
QUESTION 2: i have error in the last two lines.
2022-10-10 6:39 AM
Dear Sir,
Unfortunately, I am not familiar with STM32 peripherals therefore I cannot help you with that.
We only support Automotive microcontrollers like SPC58.
Thank you in advance for your understanding.
Best Regards,
AutoDevKit Team