Question
TDA7498E
Posted on January 24, 2017 at 10:22
As we know, TDA7498E is designed for Audio amplifier application. But we are interested in using it for DC amplifier application.
In our application, an inductance coil is connected to amplifier output. This load is up to 24VDC / 3A max, so Class D amplifier is idea for it.
But the operating frequency range is from 0Hz-100Hz, which is different with Audio application. Can we just remove the DC-block capacitor from the input circuit, and use TDA7498E in this DC amplifier application?
#tda7498e