2023-05-15 11:31 PM
IRF520 type MOSFETs are starting to be phased out and so in all review, STP16NF06 should be a stable cross reference from what I have read, would anyone know perhaps is there a better cross for an IRF520 than the ST STP16NF06? i have ask OnSemi and their idea on this question is not much help as they point to MOSFETs that actually lower in current and PD
2023-05-16 12:54 AM
Welcome, @MRUEF.1, to the community!
You are obviously using the IRF560 in the TO-220 package variant, right?
I know this MOSFET with a maximum drain voltage of 100V, Rdson max 0.2ohms and a continuous current of max 6.8A at 100°C.
The STP16NF06 you have chosen can only handle 60V, but more current with a smaller Rdson.
For max 100V I rather recommend the STP24NF10 with 100V, max 0.06ohms and 18A at 100°C. There are many more suitable types with considerably better parameters, but a more precise selection only makes sense if you know your application and exact requirements (frequency, driving, etc).
Hope that helps?
Regards
/Peter