2016-10-17 7:49 AM
Hey there,
i have problems to choose the right input setting of the STA309A. My current input is I2S with 48 samples at 512*fs. The sites 22-25 of the datasheet are a bit confusing. In CONFA i can choose a MSC e.g. of 48 samples with 512*fs. But at page 25 i only can choose a maximum of 64*fs for I2S input sound formats. What is the difference between those registers and settings? Which configuration now is the right one? I have a XTI input of 24.576 MHz at the ADC's and the DSP. Greetings!2016-11-15 12:30 AM
hi ME,
STA309A can handle 192Khz sample rate .
according to your hardware configuration, please make sure your bit clock is 12.288Mhz ,due to it's 64FS .
and your clock output frequency is strange , please check your PLL networks parameters , is it aligned with ST recommended application circuitry .
by the way, please down load APWorkbench from ST website, this tools will help you to initialize STA309A properly .
Thanks
YT