2020-04-15 7:13 AM
Hi all,
I'm conducting a project which require to Wireless Internet 3G: a remote speaker that can receive and broadcast audio file from a server. Until now, I have listed out some basic criteria for MCU selection mostly relating to peripherals requirements, such as: SDIO for SD card, I2S for audio, Ethernet and UART for Internet connection, STM32 MCU (cuz I'm familiar with it).
For these general requirements, many MCUs are able to adapt. So I need to list a more specific criteria.
Could you guys suggest me which items do I need to focus ( SRAM, Flash memory, clock speed ...) ?
Currently, I'm considering STM32F437VGT6, but I'm not sure it have enough power to run reliably or not ?
I know it quite of general, but if you need more information about my project, pls raise a question.
Solved! Go to Solution.
2020-04-16 12:25 AM
Hey,
Using SAI/I2S at 48 Khz samplilng frequency and external codec (2xADCs + 2xDACs), CPU at 168 Mhz, every 700uS DMA interrupt is generated
and 128 words buffer is needed for the samples. This is off course stereo going both directions.
How is the 3G modem connected to the STM32 ? Where is the internet stack implemented ? Inside the modem or locally on the STM32 with lwIP.
I see the bottleneck here the connection between the modem and the STM32, also 3G means variable speed, which at point can get lower than
the I2S bandwidth, this means you need some buffer RAM for your audio file, assume it is streamed. Depending on how big your audio file is,
the internal RAM might not be enough, especially if you implement lwIP stack inside the CPU.
Is this hardware player for Internet Radio ? You also need the STM32 to handle LCD/UI ? Or some public announcement system, where you can
go with mono audio, download the audio file to a SD card and play it later ?
2020-04-15 3:30 PM
Does anyone have any idea about this ???
2020-04-16 12:25 AM
Hey,
Using SAI/I2S at 48 Khz samplilng frequency and external codec (2xADCs + 2xDACs), CPU at 168 Mhz, every 700uS DMA interrupt is generated
and 128 words buffer is needed for the samples. This is off course stereo going both directions.
How is the 3G modem connected to the STM32 ? Where is the internet stack implemented ? Inside the modem or locally on the STM32 with lwIP.
I see the bottleneck here the connection between the modem and the STM32, also 3G means variable speed, which at point can get lower than
the I2S bandwidth, this means you need some buffer RAM for your audio file, assume it is streamed. Depending on how big your audio file is,
the internal RAM might not be enough, especially if you implement lwIP stack inside the CPU.
Is this hardware player for Internet Radio ? You also need the STM32 to handle LCD/UI ? Or some public announcement system, where you can
go with mono audio, download the audio file to a SD card and play it later ?
2020-04-16 8:56 AM
Firstly, thank you for your reply. OMG, at last some one read my post . Could you go into more details instructions about this:
Looking forward your reply, bro
2020-04-16 9:32 PM
Hi MONKA,
Maybe my ask not clear enough.
It like a internet radio and send/receive data through MQTT broker.
After receiving audio file, it will broadcast through a speaker.