Difference between LM224 and LM224A
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-11-28 12:04 AM
Posted on November 28, 2014 at 09:04
Hi,
Is there tmeperature drift difference between the two types? Or is there any other difference between the two type,please? Thanks!
Labels:
- Labels:
-
Operational Amplifiers
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-11-28 2:38 AM
Posted on November 28, 2014 at 11:38
Hi wang.zhen.003,
For most of ST operational amplifier product the A label define a product with a better Vio.
You don’t have any difference one the DVio/DT = 7µV/°C in typical value or 30µV/°C for max value in the both cases.
If you compare the max Vio value between LM224 and LM224A you can see a difference of 2mV.
Ambient:5mV -> 3mV(A version)
Temperature:
7mV -> 5mV(A version)
Regards
Florian