cancel
Showing results for 
Search instead for 
Did you mean: 

Correct use of SMR (Sound MeteR) library

Fib
Associate II

Hello.

I'm trying to import the SMR module of the X-CUBE-AUDIO package in one of the projects I am working on. I wish to know the sound pressure level in dB on my microphones.

My application generates a PCM buffer filled this way: 32 samples in 16-bit format (16 samples for each channel). The sampling frequency is 16 kHz.

It seems that everything is set rightly but, when i call the smr_process function, the application goes in Hard Fault.

I am following the API call procedure shown in UM2031, pp. 16-17 (file attached).

Anyone could please help me understand what I'm doing wrong?

Below there's part of the code I am using.

The project runs on STM32F767 MCU.

/* SMR Manager */
void *pSmrPersistentMem = NULL;
void *pSmrScratchMem = NULL;
 
static smr_static_param_t smr_static_param;
static smr_dynamic_param_t smr_dynamic_param;
 
static buffer_t BufferHandler;
static buffer_t *pBufferHandler = &BufferHandler;
 
uint16_t PCM_Data_SMR[32]; 		/* PCM data buffer */
 
 
void AudioSMR_Init()
{
     int32_t error = SMR_ERROR_NONE;
  
     /* Allocat mem for Smr */
     pSmrPersistentMem = malloc(smr_persistent_mem_size); 	/* 0x188 */
     pSmrScratchMem = malloc(smr_scratch_mem_size);       	/* 0xF04 */
 
     /* Effect Initialization and configuration */
     /*-----------------------------------------*/
     /* Enables and resets CRC-32 from STM32 HW */
     __HAL_RCC_CRC_CLK_ENABLE();
     CRC->CR = CRC_CR_RESET;
 
    /* SMR effect reset */
    smr_reset(pSmrPersistentMem, pSmrScratchMem);
 
    /* SMR effect static parameters setting */
    smr_static_param.sampling_rate =16000;   			/* only sampling rate supported */
 
    smr_setParam(&smr_static_param, pSmrPersistentMem);
   
    /* SMR dynamic parameters that can be updated here every frame if required */
    smr_dynamic_param.enable = 1;		/* SMR module enabler */
    smr_dynamic_param.averaging_time = 100;
    smr_dynamic_param.filter_type = SMR_PREFILTER_NONE;
 
    smr_setConfig(&smr_dynamic_param, pSmrPersistentMem);
 
    /* I/O buffers settings */
    BufferHandler.nb_bytes_per_Sample = 2;			/* 16-bit */
    BufferHandler.nb_channels = 2; 					/* stereo */
    BufferHandler.data_ptr = PCM_Data_SMR;
    BufferHandler.buffer_size = 32/2; 		/* just half buffer is process (size per channel) */
    BufferHandler.mode = INTERLEAVED;
}
 
 
void AudioSMR_Process()
{
     int32_t error = SMR_ERROR_NONE;
     uint32_t sample = 0;
 
     /* output signal power sent to terminal IO */
     smr_getConfig(&smr_dynamic_param, pSmrPersistentMem);
 
     smr_process(pBufferHandler, pBufferHandler, pSmrPersistentMem);
 
     /* output signal power sent to terminal IO */
     smr_getConfig(&smr_dynamic_param, pSmrPersistentMem);
 
     printf("Left  mean power=%ld dB\n", (int32_t) ( (float) smr_dynamic_param.mean_level_left*0.25) );
     printf("Right mean power=%ld dB\n", (int32_t) ( (float) smr_dynamic_param.mean_level_right*0.25));
}

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
jeantil88
Associate II

I am not an expert for this, but I think I read somewhere that it only support 48 kHz sampling frequency.

MReyn
Associate II

Did you ever managed to get this to work? I'm trying to implement the same library but i have exactly the same error.