cancel
Showing results for 
Search instead for 
Did you mean: 

Best Low Power buffer op amp

JWeij.1
Associate II

I need to measure a signal with very low power, the signal can range anywhere between -1 and +10 Volts but i only need the 0 to 3volts for my ADC input(my battery is also 3V). is there an opamp that fits my requirements that is less than 50uA?

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 REPLY 1
MikeDB
Lead