2016-08-10 9:11 AM
hi,
I had some questions when i use the TDA7492P. When I turn on the 12V power(connect to the PVCC)and don't connect the 5V(connect to the SVCC), the pin1 of TDA7492P willimmediately
burn( the pin1 will short with pin2/pin3) . I don't connect the L2~L9 and thespeaker。
I had test 4pcs TDA7492P, they are all this case。2016-08-22 6:59 PM
your application circuitry is wrong , SVCC must be connected with a capacitor between VSS. rather than external power supply .
please follow the application schematic in datasheet .
you can find it in below link.
Thanks
YT