Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
I have STM32WB55 Nucleo Development Kit. I am trying to understand how to use Zigbee. I need to create "Centralised Network" and transmit data from End Devices to Server. How can I transmit data? Does any examples to transmit data from End Device to Server?Also will be helpfull any "Application notes", "User manuals".
Hi,In a BLE mesh, I want to send vendor commands from the vendor client node to the vendor server node and get responses and notifications from the server node. I also need to set the publish and subscribe addresses of the vendor client node.But there isn't any vendor client in the SDK. I tried to implement it but there is no effect.How do I test it ? or is there any way I can develop it ?or is it going to be available in next commit or so ?Kindly help me.Thanks.
..
Hi, I wanna use STM32WL for 148-152Mhz. But I cannot out 13dBm power for RFO_LP.If anyone know Zopt impedance for 150MHz ins this IC, you let me know it. Off course 169MHz is no problem. Almost of application note is written over 433MHz.Thanks.
Is it possible to integrate BLE OTA functionalities into BLE LLD projects? For example, we would like to make the BLE_LLD_Proximity example OTA compatibile, which however requires the FW stm32wb5x_BLE_LLD_fw.bin, while the BLE Ota bootloader example requires the FW stm32wb5x_BLE_Stack_full_fw.bin to work. Or is there a Ble Ota LLD example project that works with FW stm32wb5x_BLE_LLD_fw.bin? Any help is greatly appreciated, thank you.
Is it possible to write a custom co-processor binaries for CPU2 instead of using the coprocessor binaries from stm
Hello,I am using p2p_server BLE example with RTC Internal Wakeup with interrupt. But somehow void RTC_WKUP_IRQHandler(void) is not getting called. Please let me know the possible reason.Regards.
Hello dear tech support and comunity.Is it possible to get sources for ST BLE Sensor 4.12.0 for Android and were?Here https://github.com/STMicroelectronics/STBlueMS_Android it seems to be only 4.9.0 as latest one.BRAlex
when the example file is modified but the original program gets recovered when the Device Configuration Tool Code Generation is hit after some changes in ioc file.#stm32wl55jcIts hard to start from the scratch in LoRa subghz, Do anyone have some methods?Thank you
I am Attaching Observed Current Consumptions. I am observing Huge Difference between claimed current value versus observed current value at various low power modes. I am having right Connections as mentioned in Power Consumption measurement board Datasheet just to measure only current consumptions at Microcontroller and not at other devices such as Regulator, STLink, SMPS and so on which are present on STM32WB55.Please Correct me if am wrong or Suggest me the exact connections to measure exact current at Microcontroller.Thanks in Advance.
I'm trying to run broadcasting mode on the base off BLE_P2PServer example and instead of aci_gap_set_discoverable in app_ble.c, in "Adv_Request" function, I'm trying to use the below function: aci_gap_set_broadcast_mode( Min_Inter, Max_Inter, ADV_NONCONN_IND, PUBLIC_ADDR, sizeof(manuf_data), manuf_data, 10, white_list_broadcasting);As a result I'm getting 0x46 = BLE_STATUS_NOT_ALLOWED.May I ask for any support of how to set the broadcasting mode?
How much flash memory is allocated for CPU2 flash and is it possible to write a RF firmware without involvement of CPU2
UART setting are shown in picture of both devices
Hello,There's a degradation in flash erase during BLE connection use-case between release 1.11.1 and 1.12.0.On 1.12.0 flash erase operation will cause the BLE client to disconnect (timeout).Same user code just the different FW version - 1.11.1 works, 1.12.0 does not. Its the same flow since the introduction SEM7 mechanism around 1.5.0 release.Tested on stm32wb5x_BLE_Stack_full_fw (STM32WB55)I couldn't find a mention for behavior change in the release notes, nor in related examples (BLE_RfWithFlash) so I assume its an unintentional issue.Thanks in advance
On the site of Rising hf i found a solution: "STM32Nucleo_ATCmd_Bridge-v0.1.3-20170920.bin". This file is impossible to find online. I tryed a usb- serial comunication with the sensor shield, but i can only recive data and not sending them. The lorawan shield of Rising hf it's impossible to reach. i don't know how can i install a new firmware on NUCLEO-L073RZ to comunicate with the module.
i am trying to implement I2C for the LPS33HW Sensor in the LoraWAN endnode application. I know that the STM32WL55JC in the IDLE Mode it is going into the STOP2 Mode. Therefore i defined the i2c3 because it can be woken up without a lose. The Clock for the I2C3 is the HSI16 because it is referred to the RM0453 reference manual.Im inizializing the I2C in the sys_app.c at the bottom of the SystemApp_Init, also i enable the Wakeup of the hi2c3 by setting the WUPEN of the register to 1.i registered the task to read a the sensor value as a schedule task, created a timer for 9000 ms and started the timer. I'm giving the value which the value has read to a global variable. After the Mac sending, the MCU is stopping and there is no process anymore. And thats the question is there something i dont see or overlook ?
Here is the function running in my STM32WB55CG:/** * this function can be nested */ void UTIL_SEQ_WaitEvt( UTIL_SEQ_bm_t evt_id_bm ) { UTIL_SEQ_bm_t event_waited_id_backup; UTIL_SEQ_bm_t current_task_id_bm; /** store in local the current_task_id_bm as the global variable CurrentTaskIdx * may be overwritten in case there are nested call of UTIL_SEQ_Run() */ current_task_id_bm = (1 << CurrentTaskIdx); /** backup the event id that was currently waited */ event_waited_id_backup = EvtWaited; EvtWaited = evt_id_bm; /** * wait for the new event * note: that means that if the previous waited event occurs, it will not exit * the while loop below. * The system is waiting only for the last waited event. * When it will go out, it will wait again fro the previous one. * It case it occurs while waiting for the second one, the while loop will exit immediately */ while((EvtSet & EvtWaited) == 0) { UTIL_SEQ_EvtIdle(current_task_id_bm, EvtWaited); } EvtSet
Hi,I am looking for an STM based MCU/kit with high accuracy crystal oscillator with possible option to fine tune the frequency. I want to use it for some high accuracy time reference. Looking for suggestion please.- ijaz
Hi,I found a possible bug in the "stm32wbxx_hal_msp.c" file when using Cube in the STM32CubeIDE to enable the SAI peripheral.I did not test all the combinations, but have mine set up as follows:SAI A - Async SlaveSAI B - Sync Slave The bug is that the the code does not include and set the "Alternate" member of the GPOI_InitStruct for SAI Block A and BThe generated code is:/**SAI1_A_Block_A GPIO Configuration PA8 ------> SAI1_SCK_A PA9 ------> SAI1_FS_A PA10 ------> SAI1_SD_A */ GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);and/**SAI1_B_Block_B GPIO Configuration PA5 ------> SAI1_SD_B */ GPIO_InitStruct.Pin = GPIO_PIN_5; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);But it sho
I am using BLE OTA bootloader found in CubeWb1.8.0 to upload a firmware to a custom STM32WB55CG device. I am using ST BLE sensor app to upload the firmware from an android phone to the custom device. I was able to successfully carry out FOTA and restart the uploaded firmware after OTA for some android phones. For some other phones, I was able to upload the firmware and get the Uploaded notification in the ST app but, the device does not restart to run the uploaded firmware in several android phones. What does that mean? Does that mean any issue with indicate characteristic enabling from those android phones?
After flashing the firmware and connecting to the uart pins, I can get some lora settings when resetting the MCU but when i try to send at-commands i get no response. Any help appreciated
Hello,I wanted to know is there any product in the market where STM32 MCUs are used in Implantable Devices. Are there any Medical Norms for STM Controllers? Can we Use STM32WB as a Implantable with BLE?Thanks in Advance.
After downloading I-CUBE-LRWAN and running the B-L072Z-LRWAN1 example i get the that LmhpCompliance.h doesn't exist but looking into the files i do see that it does exist. Any help appreciated.
What was known as "The Things Network" (TTN) is now "legacy" and not accepting any new devices, gateways, or applications. Thus, I think, all ST materials referencing "The Things Network" are now obsolete & unusable.So, has anyone managed to migrate anything based on I-Cube-LRWAN to the new "Things Stack" aka "V3" ?
I am trying to start HSE with external crystal (on nucleo WL55JC1 board). I removed R2 (Output from TCXO), added two 0E bridges R39 and R40, added 10k resistor R41 (to remove stub). Then I started the Cube-MX (latest, fresh update...), selected the nucleo WL55 from the board selector, initialized the periphery with board, changed RCC HSE settings to Crystal/Ceramic Resonator and changed the clock configuration to When I compile and debug the project generated by Cube, the execution quits in error handler when the __HAL_RCC_GET_SYSCLK_SOURCE() is called (stm32wlxx_hal_rcc.c, line 347). The HSE status in RCC Control register remains 0 (HSE not ready). Then I checked ref. manual and set all registers "by hand", using only CMSIS calls to enable HSE without success either. With "out of factory" Nucleo setup (TCXO) and settings to use TCXO, everything runs normally. Is there anything else I am missing here? Is there working example with STM32WL or WLE using external XTAL ?Thanks!Marko
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.