Skip to main content
IAhma.1
Associate II
Aug 5, 2021 4:40 PM UTC
Question

STM32 Kit with high accuracy crystal

Hi,

I am looking for an STM based MCU/kit with high accuracy crystal oscillator with possible option to fine tune the frequency. I want to use it for some high accuracy time reference. Looking for suggestion please.

- ijaz

This topic has been closed for replies.

13 replies

TDK
Aug 5, 2021 5:24 PM UTC

Crystals are high accuracy by their very nature. As long as it uses one, it should be accurate to tens of ppm. What accuracy do you need?

The STM32H7 series can use fractional PLL loop to further tune the clock.

This uses a crystal (NX3225GD-8MHz-EXS00A-CG04874) accurate to ±20 ppm. Probably can't get much better with ST boards.

https://www.st.com/en/evaluation-tools/nucleo-h743zi.html

"If you feel a post has answered your question, please click ""Accept as Solution""."
IAhma.1
IAhma.1Author
Associate II
Aug 5, 2021 6:29 PM UTC

Actually I need a board with stable oscillator from 0-degree to 50-degree temperature. I want to measure accurate signal time over 12hrz. I heard that normal crystal oscillators have some variations over temperature. A board I know is STM32WB which i guess provide crystal tuning.

TDK
Aug 5, 2021 6:31 PM UTC
Everything has variation over temperature. There is no perfect clock source. You haven’t answered what amount of error is acceptable to you. “No error�? is not an option.
"If you feel a post has answered your question, please click ""Accept as Solution""."
Uwe Bonnes
Chief
Aug 5, 2021 5:25 PM UTC

Define "hifg accuracy" and "fine tune range"

Tesla DeLorean
Guru
Aug 5, 2021 5:48 PM UTC

Cause some of us have higher standards than others..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
IAhma.1
IAhma.1Author
Associate II
Aug 5, 2021 6:30 PM UTC

I want to measure accurate signal time over 12hrz. I heard that normal crystal oscillators have some variations over temperature.

Tesla DeLorean
Guru
Aug 5, 2021 5:42 PM UTC

Can't you just mount a VCTCXO ? How hard can that be? Wire it to a DAC with a LPF.

SiTime has a part you can trim via I2C

How about using a LEA-M8F, clocking the STM32 with the 30.72 MHz? GNSS locked that's good to 5ppb

The Murata module here claims to have a TCXO +/- 2ppm, near term probably a fraction of that.

https://www.st.com/en/evaluation-tools/b-l072z-lrwan1.html

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
IAhma.1
IAhma.1Author
Associate II
Aug 5, 2021 6:34 PM UTC

Actually I want to measure a signal time over 12hrz long via STm32 timer. for that purpose I need a reference board with stable XTL frequency.