Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Hello,I'm working on a project using Zigbee as main communication network.In this project we develop two devices :One as server and coordinatorOne as client and routerWe based our hardware on STM32WB5MMG.I used the examples of Zigbee_OnOff_Client_Router and Zigbee_OnOff_Server_Coord to understand how to develop our application.I'm actually stuck at a point where mu client router cannot connect to the coordinator and the join status is ZB_APS_STATUS_SECURITY_FAIL.I don't know how to solve this error, the preconfiguredLinkKey are the same, exactly as in the examples.I think the problem come from the coordinator because if I use the coord example in a nucleo board, my router device is able to connect to it... but I haven't been able to find th differences between my coord and the example and I can't find a lot of documentation on how to debug this kind off errors.Can anybody help me ?Thanks in advance and have a nice day.
I have P-NUCLEO-WB55 it worked initially well with BLE stack. Later I have ported Zigbee Stack but things were not working out. I went back and loaded the BLE stack now, but it is not even advertising with p2p sever application. I have tested the GPIO and UART functions works well. But only the RF is not seems getting activated. I have tried erasing chip and loading the stack and app freshly from pre-built images (not working)I have reinstalled the FUS through cubemx programmer but did not helped.I tried loading transparent mode application, but it is not connecting to virtual COM port detected in STMCube RF monitor tool as well ?The USB dongle came with kit works fine but the Nucleo board is not working. Is there any way to restore the board to factory default ?If RF is not working means, some thing wrong with Hardware ?
Hi All, I'm currently using an STM32WB5MMG module on two devices to establish a Zigbee connection between them.My project is based on the example called "BLE_Zigbee_Dyn"(one device should also be able t communicate using BLE ) implementing everything over an RTOS environment.On Zigbee network One works as a Coordinator and the other is the end device; Both are configured to have two endpoint : one Switch endpoint (to manage a toogle and a polling system ) and one Level Endpoint (to Manage the behaviour of the coordinator device)Below the code for the configuration of the two endpointsstatic void APP_ZIGBEE_ConfigEndpoints(void) { struct ZbApsmeAddEndpointReqT req; struct ZbApsmeAddEndpointConfT conf; memset(&req, 0, sizeof(req)); req.profileId = ZCL_PROFILE_HOME_AUTOMATION; req.deviceId = ZCL_DEVICE_ONOFF_SWITCH; /* Endpoint: SW1_ENDPOINT */ req.endpoint = SW1_ENDPOINT; ZbZclAddEndpoint(zigbee_app_info.zb, &req, &conf); //assert(conf.status == ZB_STAT
Hi all,I'm trying to develop on the Nucleo USB dongle. I'm creating an empty Zigbee project with the FW 1.12.1 I configure the minimum in cubeMX the project crash in startup_stm32wb55cgux.s I'm running FUS V1.2.0.0I'm using the wireless copro : stm32wb5x_Zigbee_FFD_fw.bin from the version 1.12is anyone able to use zigbee on the STM32WB55CG ?Thank youRegards
..
I'm trying to get a handle on using the Sub Ghz middleware along with the processor's low power modes. I've configured an X-NUCLEO-LPM01A to power the NUCLEO-WL55JC, following the instructions from the STM32WL webinar, so I can take some measurements. I'm using LPTIM1 to generate an interrupt every 4 s where I then transmit a short packet with the radio configured for FSK modulation. The radio is set to sleepmode in the TX complete callback. and the processor set to enter stop 2 mode again. For the first time the board is powered down in STOP 2, I measure the expected 2.5 uA, but as soon as the first radio packet is sent, the current doesn't go below 650 uA. (See the attached screenshot)Does anyone have any insight as to what it could be? It seems to me that something is preventing the processor from entering the STOP 2 mode again. Could it be an unhandled interrupt? I also can't tell if the radio is set to sleep successfully after that first transmit. Any assistance would be greatly a
I'm trying to use Pa7 for an external falling edge irq without success. I have pb1 and pb4 working as expected, but not Pa7. Is there anything special about using EXTI9_5_IRQn vector?
The content of the function is simply putting data in the buffer and sending it.Even if the function is called once, it sends data 2 to 4 times.However, looking at the logs from the LORA gateway, they are sending data continuously.I'm not sure why these issues arise.The connection type is ABP mode.It is transmitted once in OTAA mode, but this problem occurs only in APB mode.P.S gateway, network, and application server are using CHIRPSTACK.
Hi I am testing with STM32WL55I programed that MCU transmitted LoRa signal periodically and transmitted data via uart1 periodically.At first, MCU can recieve data via uart1.After a certain amount of time, MCU can't transmitted some bytes via uart1 once or twiceand then MCU can't receive data via uart1 continuously.I don't know how to fix the problem.1. init /* Initialize all configured peripherals */ MX_GPIO_Init();// MX_I2C2_Init(); MX_SUBGHZ_Init(); MX_USART1_UART_Init(); MX_USART2_UART_Init(); MX_I2C3_Init(); MX_RTC_Init(); MX_TIM16_Init(); /* USER CODE BEGIN 2 */ MX_SubGHz_Phy_Init(); MX_I2C2_Init(); HAL_TIM_Base_Start_IT(&htim16); init();2. I used timer_if.c : see added files3. transmitted data via uart1The red line indicates the part where the data is not completely transmitted.4. I add the project. please check where the problems are and let me know how to fix them.thank you
I have some questions on the response here:https://community.st.com/s/global-search/MLPF-WB55-02E3?t=1636577804470The response references MLPF-WB55-01E3 but I think it should be MLPF-WB55-02E3 for the WLCSP_100 package. Can you confirm the 65 ohm impedance is correct for the MLPF-WB55-02E3 filter?I am using a different stack-up than the one in the MLPF-WB55-02E3 datasheet. I will implement a 65 ohm CPW for our stack-up. Once that is done is there still a requirement to maintain a trace length of 1.5 mm? Thanks.
Hello ST,I am using STM32WB55 board to establish mesh network between four node. Duration of provisioning from provision node taking long time (>25 sec ) and some time my command was correct " atep prvn0 2".. even UART is showing process is complete but LPN node led is not responding. Out of 10, only 6 times process working correctly & blue led is responding. Provisioning process is very long for any multiple node application if node did not configured properly it goes for long time processes to ensure that all node in network is working or not. I have put lots of effort to reduce the provisioning time period for one node but didn't get success . Please provide me guidance for this...Best RegardsDeepak Aagri
Hi,I'm working on the two MCU's STM32WLE5C8U6 & STM32WLE4CCU6 and I need to know the UID in order to indentify each of the products.In the doc it's written that both have UID but there is no address to read them.What I'm missing ?Best regards,
Hi,I am using STM32WB55 to develop a PHY 802.15.4 application with custom MAC. I found only the Phy_802_15_4_Cli example, but there are ASCII like commands. Can you provide byte oriented commands for working with PHY?
I am attempting to send a file via BLE (Windows app -> STM32WB55), I've found that the ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE event is called whenever a packet is received by the board however I am unable to find where the actual packet data is stored or understand how to output it. (I.e. send "HELLO" string via BLE, board outputs "HELLO" via uart).I am trying to output this data serially via the UART connection. Similarly, I am trying to receive input via uart and transfer the payload from the board to the windows app via BLE. I have looked at attribute_modified->Attr_Data and similar variables within the event, however I don't believe these are what I'm after. Thank you for any help,Oliver.
I have a simple example where I take an A/D sample from a pot every 15ms. I then modify CCR1-4 on both TIM2 and TIM1 AS WELL AS ARR registers on TIM2 and TIM1. ARR is updated with a value and ALL CCRx are updated with that value - #define. I notice that TIM1 works just fine but TIM2 CNT seems to go "out of bounds" past ARR value. The HW is an STM32WB55 that is on a dev board by Midatronics (Sharky Mkr). Both timers are set up identical except for Tim2 missing registers(see below). Can someone tell me what I might be missing here?Configuration looks like (most of this comes from CubeMx:static void MX_TIM1_Init(void) { /* USER CODE BEGIN TIM1_Init 0 */ /* USER CODE END TIM1_Init 0 */ TIM_MasterConfigTypeDef sMasterConfig = {0}; TIM_OC_InitTypeDef sConfigOC = {0}; TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0}; /* USER CODE BEGIN TIM1_Init 1 */ /* USER CODE END TIM1_Init 1 */ htim1.Instance = TIM1; htim1.Init.Prescaler = 1600 - 1; ht
For the new STM32WB10CC chip, there is no specification on default state of the RF pin, however, it should not be shorted to GND. Hardware has been verified with high confidence that short is not due to physical issues, is software short to GND on RF1 possible and how would one verify?
Hi, I recently read the AN5165——Development of RF hardware using STM32WB microcontrollers,and the page25~page27 show the STM32WB55's reference design.But I didn't find the file on the offical website.Could you please share the files named:MB1427A---UFQFPN48MB1422A---VFQFPN68MB1547B---UFBGA129MB1425A---WLCSP100Thank you very much.
I enable counter by __HAL_TIM_ENABLE(&htim17);and I see in debugger that PSC register incrementing, not CNT. CNT is always zero. Are the registers messed up?Settings are from CubeIDE 1.41 with stm32wb pack 1.8:static void MX_TIM17_Init(void){ /* USER CODE BEGIN TIM17_Init 0 */ /* USER CODE END TIM17_Init 0 */ /* USER CODE BEGIN TIM17_Init 1 */ /* USER CODE END TIM17_Init 1 */ htim17.Instance = TIM17; htim17.Init.Prescaler = 0; htim17.Init.CounterMode = TIM_COUNTERMODE_UP; htim17.Init.Period = 65535; htim17.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim17.Init.RepetitionCounter = 0; htim17.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_Base_Init(&htim17) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM17_Init 2 */ /* USER CODE END TIM17_Init 2 */}
Hi everyone.I use End-Node example code in I-Cube-LRWAN software to run I-Nucleo-LRWAN1, but my device always say join fail.I learn to this video step by step do, but also not work.Conld anyone can help me? Thank you.Update 2021/11/12The End-Node example code in I-Cube-LRWAN is not for I-Nucleo-LRWAN expansion board. It's for SX1272MB2DAS expansion board. So if you use I-Nucleo-LRWAN expansion board you only can use LoRaWAN_AT_Master example code in I-Cube-LRWAN.
Hello, i'm using the NUCLEO-WL55JC board.I am using the LoRaWAN_End_Node example which works fine. However I reach an operating current of around 50mA.Do you have an idea for a solution?Have a good day !
Does anyone know how to restore the default settings of the dongle MB1293C? I was testing it and I did something to it that I didn't notice about and now my computer only recognizes the dongle whet the dongle is in Boot0 mode. Moreover, any LED is on or blinking.
HelloI use STM32CubeProg 1.6 to configure my stm32wb55. If I use ST-Link there are two bookmarks and if I use USB boot there is only one bookmark. Is it ok? And also there are a lot of error while I try to set option bytes via ST_Link. P.S. Please make CubeProg GUI a part of CubeIDE. @Imen DAHMEN
Hi Community,I'm using B-L072Z-LRWAN1 using the firmware AT slave available in the package en.i-cube_lrwan. The evaluation board uses the module CMWX1ZZABZ-091 that includes STM32L072 but the commercialized version of the module is CMWX1ZZABZ-078 that includes STM32L082 with integrated AES-128. I need therefore to migrate the AT slave firmware from STM32L072 to STM32L082. Does anyone have experience with this activity? Is it enough to rebuild the project with STM32L082 (and not use the AES-128 hardware accelerator) or other firmware changes are necessary?Thanks in advance for the support.Matteo
Hello there. I have the NUCLEO-WL55JC1 board. But I couldn't get it to work. The errors I get when I try to connect to ST-LINK Utility and load code in CubeMX are available in the pictures. Can you help me to solve these problems?
I am working on a lorawan project targeted at STM32WB55CGT6. It is QFN48 and I tried running the successful project on NUCLEO-WB55CG. The development board is QFN64. Would I be able to use the same Nucleo board for further development for STM32WB55CGT6? In addition, what is the difference between P-NUCLEO-WB55CG and NUCLEO-WB55CG? Please suggest to me the best evk for STM32WB55CGT6. Thanks in advance
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.