Skip to main content
SYun.2
Associate II
Nov 11, 2021 5:12 AM UTC
Question

Once SendTxData function is called in "I-CUBE-LRWAN 2.0.0", it is called continuously.

The content of the function is simply putting data in the buffer and sending it.

Even if the function is called once, it sends data 2 to 4 times.

However, looking at the logs from the LORA gateway, they are sending data continuously.

I'm not sure why these issues arise.

The connection type is ABP mode.

It is transmitted once in OTAA mode, but this problem occurs only in APB mode.

P.S gateway, network, and application server are using CHIRPSTACK.

This topic has been closed for replies.