Skip to main content
PMana.1
Associate II
Nov 8, 2021 10:45 AM UTC
Question

Which EVK should be used for STM32WB55CG.

I am working on a lorawan project targeted at STM32WB55CGT6. It is QFN48 and I tried running the successful project on NUCLEO-WB55CG. The development board is QFN64. Would I be able to use the same Nucleo board for further development for STM32WB55CGT6? In addition, what is the difference between P-NUCLEO-WB55CG and NUCLEO-WB55CG? Please suggest to me the best evk for STM32WB55CGT6.

Thanks in advance

This topic has been closed for replies.

2 replies

ST Employee
Nov 8, 2021 12:09 PM UTC

Hello @PMana.1​ 

Lorawan device is supported by default on STM32WL not on STM32WB (BLE). There is 2 version of the nucleo board depending of the targeted frequency (433MHz/868MHz).

Is you project trying the LoRa @ 2.4GHz ?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PMana.1
PMana.1Author
Associate II
Nov 8, 2021 1:08 PM UTC

Hi, I am using LR1110 and I need bluetooth too. so the chip is stm32wb55. I can't make change on the mcu selected. I just want to know, which development board should I use.. Thanks