Skip to main content
LMesn.1
Associate
Nov 4, 2021 7:28 AM UTC
Solved

How to reduce current consumption on NUCLEO-WL55JC ?

Hello, i'm using the NUCLEO-WL55JC board.

I am using the LoRaWAN_End_Node example which works fine. However I reach an operating current of around 50mA.

Do you have an idea for a solution?

Have a good day !

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Nov 4, 2021 8:04 PM UTC

Hello @LMesn.1​ ,

The following features are implemented to reduce the current consumption:

  • The core logic is supplied by the low-power voltage regulator to reduce the quiescent current.
  • The Flash memory can be switched off (power-down mode and clock gating) in LPSleep mode. The Flash memory can also be switched off in LPRun mode when the application processor executes from SRAM1.
  • The system clock is limited to 2 MHz. The MSI internal RC oscillator can be selected as it supports several frequency ranges, with a small device total consumption (such as 48 µA in LPSleep, Flash memory off, at 100 kHz). 

Please refer to this AN5568 "Ultra-low-power features of STM32WL Series microcontrollers", it may be helpful for you.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

3 replies

Imen.DBest answer
ST Technical Moderator
Nov 4, 2021 8:04 PM UTC

Hello @LMesn.1​ ,

The following features are implemented to reduce the current consumption:

  • The core logic is supplied by the low-power voltage regulator to reduce the quiescent current.
  • The Flash memory can be switched off (power-down mode and clock gating) in LPSleep mode. The Flash memory can also be switched off in LPRun mode when the application processor executes from SRAM1.
  • The system clock is limited to 2 MHz. The MSI internal RC oscillator can be selected as it supports several frequency ranges, with a small device total consumption (such as 48 µA in LPSleep, Flash memory off, at 100 kHz). 

Please refer to this AN5568 "Ultra-low-power features of STM32WL Series microcontrollers", it may be helpful for you.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
LMesn.1
LMesn.1Author
Associate
Nov 7, 2021 9:37 AM UTC

Thank you very much, i will try all of this.

Have a good day.

LMesn.1
LMesn.1Author
Associate
Nov 9, 2021 8:54 AM UTC

Hello i applied your advice, and i also changed the supply mode and everything is good. Thank you !