Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
The following function aci_gap_update_adv_data returns the error 0x91 which means "Failed". We don't understand why we have this error and the startup of the device. Do you have any idea ?Best regards,Audrey
Hi, I made my first steps in ZigBee by using the NUCLEO-STM32WB55 board with the USB dongle. The dongle is flashed and the blue LED is shining, but the NUCLEO board is printing the following message: [M4 APPLICATION] ZbStartup Callback (status = 0xca) [M4 APPLICATION] Startup failed, attempting again after a short delay (500 ms) [M4 APPLICATION] Network config : APP_STARTUP_CENTRALIZED_ROUTER [M0] [00000000.517][PLATFORM] ZbNlmeResetReq : NLME-RESET.request (warmStart = 0) [M0] [00000000.018][PLATFORM] zb_startup_join_nwk_disc : Attempting network discovery. Scans = 3, Duration = 4 [M0] [00000000.019][PLATFORM] nwk_scan_req : MLME-SCAN.request (wpan0): type=1, page=0, mask=0x00002000, dur=4 [M0] [00000000.031][PLATFORM] nwk_handle_beacon_ind : BEACON addr16=0x0000, epid=0x0080e125004ca76a, ch=13, pan=0x4aa2, depth= 0, lqi=192, cost=1, pjoin=0 [M0] [00000000.290][PLATFORM] nwk_scan_req : MLME-SCAN.request (wpan0): type=1, page=0, mask=0x00002000, dur=4 [M0] [0
Hello, This has happened before (here) and was fixed, but it seems that it is happening again.When the downloaded .zip file is opened with a text editor, the contents is:"Service unavailable, please try again later"Please can someone take a look at this? If this is going to happen over and over again, perhaps an alternative method of getting SigFox credentials can be created?
I did not find a real UserManual for STM32WB55, with the register-definitions, peripheral explanations etc.?
Hi,is there an error in the datasheet? The data seems counterintuitive:FT pin input leakage current (max.) is- 150 nA for 0 to VDD-2500 nA for VDD to VDD+1V-250 nA for VDD+1V to 5,5VShouldn´t the last value be in uA perhaps?Kind regardsRené
Looking for CAD resources of NUCLEO-WBA52CG board. I couldn't find any of the CAD files for the STM32WBA chips. Please guide me in this... I have the NUCLEO-WBA52CG board but It will be useful for me if I have CAD files of the Board.
Hello,i am trying to get reporting from a remote temperature sensor Server ( End device) is use ZbZclAttrReportConfigReq to acheive it. I got a STATUS SUCCES in the callback but the device never send its temperature. Can you tell me if i miss someting ? Here is my codeBestenum ZclStatusCodeT status; struct ZbZclAttrReportConfigT config; config.dst.mode = ZB_APSDE_ADDRMODE_SHORT; config.dst.nwkAddr = AT_GetParam1_hex(); config.dst.endpoint = AT_GetParam2_hex(); config.num_records = 1; config.record_list[0].direction = ZCL_REPORT_DIRECTION_NORMAL; config.record_list[0].attr_id = 0; // Temperature ID is Zero config.record_list[0].timeout_period = 30; config.record_list[0].attr_type = ZCL_DATATYPE_GENERAL_16BIT; config.record_list[0].min = 5; config.record_list[0].max = 10; config.record_list[0].change = 0.1; status = ZbZclAttrReportConfigReq( getAppInfo()->temp_meas_client, &config, AT_attReportCb, NULL );
Attached is my demo project for the NUCLEO-WB55RG dev kit.I'm trying to report ZCL_TEMP_MEAS_ATTR_MEAS_VAL when the attribute value is changed (button 3 pressed), but according to wireshark, nothing is send.See app_zigbee.c, line 329I can correctly read the value from the coordinator.What's wrong here?
static void SendTxData(void){/* USER CODE BEGIN SendTxData_1 */uint16_t pressure = 0;int16_t temperature = 0;sensor_t sensor_data;UTIL_TIMER_Time_t nextTxIn = 0; #ifdef CAYENNE_LPPuint8_t channel = 0;#elseuint16_t humidity = 0;uint32_t i = 0;int32_t latitude = 0;int32_t longitude = 0;uint16_t altitudeGps = 0;#endif /* CAYENNE_LPP */ // EnvSensors_Read(&sensor_data);temperature = (SYS_GetTemperatureLevel() >> 8);pressure = (uint16_t)(sensor_data.pressure * 100 / 10); /* in hPa / 10 */float Temp = Get_temperature(); // function reads temperature from sensorAppData.Port = LORAWAN_USER_APP_PORT; #ifdef CAYENNE_LPPCayenneLppReset();CayenneLppAddBarometricPressure(channel++, pressure);CayenneLppAddTemperature(channel++, temperature);CayenneLppAddRelativeHumidity(channel++, (uint16_t)(sensor_data.humidity)); if ((LmHandlerParams.ActiveRegion != LORAMAC_REGION_US915) && (LmHandlerParams.ActiveRegion != LORAMAC_REGION_AU915)&& (LmHandlerParams.Activ
Hi, I am working with a NUCLEO-WB15CC and can't erase all of the 320 KBytes Flash. When using the STM32_Programmer_CLI the following works perfectly fine:STM32_Programmer_CLI.exe -c port=SWD -e [0 55]but withSTM32_Programmer_CLI.exe -c port=SWD -e [0 56]or any other value larger than 55 of the upper sector index, I get the error messageError: Sector erase operation failed at least for one of the existing specified sectorsI already tried to reset the board to factory settings (as proposed in other posts) bySTM32_Programmer_CLI.exe -c port=SWD reset=HWrst -w32 0x5800040c 0x00008000This didn't help and I'm running out of ideas. Any suggestions? Thanks in advance.--Enclosed is the output of the command to display the option bytes bySTM32_Programmer_CLI.exe -c port=SWD -ob displ-------------------------------------------------------------------STM32CubeProgrammer v2.12.0-------------------------------------------------------------------ST-LINK SN : 066EFF363946433043082412ST-LINK FW : V2J37
hi all,I'm working on a STM32WB5MMGHX and I have play with p2p demos and otherI'm trying now to build a Battery service with only a battery level caracteristicI've set the caracteristic as shown belowmy custom app event handler is as folow : void Custom_STM_App_Notification(Custom_STM_App_Notification_evt_t *pNotification) { /* USER CODE BEGIN CUSTOM_STM_App_Notification_1 */ /* USER CODE END CUSTOM_STM_App_Notification_1 */ switch (pNotification->Custom_Evt_Opcode) { /* USER CODE BEGIN CUSTOM_STM_App_Notification_Custom_Evt_Opcode */ /* USER CODE END CUSTOM_STM_App_Notification_Custom_Evt_Opcode */ /* BatteryService */ case CUSTOM_STM_BATT_LVL_READ_EVT: /* USER CODE BEGIN CUSTOM_STM_BATT_LVL_READ_EVT */ APP_BATT_Single_Action(); /* USER CODE END CUSTOM_STM_BATT_LVL_READ_EVT */ break; case CUSTOM_STM_BATT_LVL_NOTIFY_ENABLED_EVT: /* USER CODE BEGIN CUSTOM_STM_BATT_LVL_NOTIFY_ENABLED_EVT */ Custom_App_Context.Batt_lvl_Notification_Status = 1; /* USER CODE END
Hi! So i have a WL55CC MCU that sends a 64 Byte Payload via LoRa to a Nucelo JC1 Board. When I'm sending with a spreading Factor of 7, everything works just fine, but with spreading factor 12 the receiver goes into a timeout mode, although I've set the RX-Timeout to 10secs and the Symbol-Timeout (?) from 7 Symbols to 12 and even 64.As you can see, the receiver starts in RX-Mode and even gets a Signal ("PRE OK"), but immidiately reaches a timeout.These are my LoRa RX settings. I'm receiving in RxBoosted mode. These are the TX-settings.Thankful for any help!Regards
When setting up the project I go to the ST url to get the ID and PAC from: https://my.st.com/sfxp the zip that is downloaded is corrupted and has a size of 0kb. I have done this procedure hundreds of times so I am sure that the problem comes from the st side. Can someone help me ? I have the production stopped... I have also created a support ticket a few days ago but nobody answer me
Sometimes, if in addition to Bluetooth, WIFI is needed in the development of a product, the third module is used. Does ST plan to include WIFI in the e.g STM32W series in the future?
Hello there!I have a request regarding PA matching impedance measurements.We are currently working on the implementation of a VHF pulsar system. Initially, we tested it on the NUCLEO board without incorporating the filtering components (impedance matching and harmonics rejection). Now, we're planning to design an RF line operating at 150 MHz with a power output of +22 dBm using the STM32WL55JCI7. I was wondering if you have access to the PA matching impedance measurements similar to the ones outlined in Annex A of AN5457. Additionally, it would be greatly appreciated if you could provide measurements at +14 dBm as well, as we'd like to test it with our current SMD Argos module equipped with an external PA could do the job with minor BOM modifications.We have designed an SMD module with an external PA for Argos TX communication, currently operating at 401.3 MHz with a power output of 26 dBm. We are looking to optimize our setup and would like to inquire if you have the PA matching imped
Hi,I am having a problem with my P-NucleoWB55 development board. When using STMCUBEIDE and trying to run the program, I get the following error.STMicroelectronics ST-LINK GDB server. Version 7.4.0Copyright (c) 2023, STMicroelectronics. All rights reserved. Starting server with the following options:Persistent Mode : DisabledLogging Level : 1Listen Port Number : 61234Status Refresh Delay : 15sVerbose Mode : DisabledSWD Debug : EnabledInitWhile : Enabled Target no device found Error in initializing ST-LINK device.Reason: No device found on target.I also cannot connect using the STM32Cube Programmer. Received following logs when tried with cube programmer.23:09:09 : ST-LINK SN : 0673FF3332584B304325481323:09:09 : ST-LINK FW : V2J35M2623:09:09 : Voltage : 0.00V23:09:09 : Error: No STM32 target found!23:39:45 : ST-LINK SN : 0673FF3332584B304325481323:39:45 : ST-LINK FW : V2J35M2623:39:45 : Voltage : 0.26V23:39:45 : Error: No STM32 target found!23:39:48 : ST-LINK SN : 0673FF33
Hello communityGateway terminal image shows FSK at channel 9 and 868 frequency.I have downloaded the library code the default set region is Europe and the frequency is 868. And I have made these changes #define USE_MODEM_LORA 1#define USE_MODEM_FSK 0to#define USE_MODEM_LORA 0#define USE_MODEM_FSK 1However, the gateway and node are not getting connected.Thank you for your help.
Good morning....Please refer to attached pics below:I have referenced Lorawan end node code from STM32 library for the STM32WL55 to use with my custom pcb that has an STM32WLE5. The RTC section of the code is identical to that in the reference code. I load the firmware onto the target and it works for a day and then locks up. Locks up is defined as no more serial comms and powering down the unit and repowering does not allow the unit to resume. If I connect with the debugger I seem to be hung in the RTC_EnterInitMode() / Hal_GetTick function. I have seen this on two boards now. Can anyone tell me what might I do and what is going on??(btw.....I do not have a structured solution on how I make it go away and rework....a myriad of rebuilding, reflashing, etc. and at some point it works again)
Hello community.What is the maximum datarate of LoRaWAN gateway?Example: If I'm sending 180,000 bytes from node to gateway, gateway will be able to transfer from node to server.?Thank you.
Hi,I configured LPUART with 57600 baudrate. With this baudrate configuration Rx interrupt stop working if I send more than 11 bytes of Data on UART. With the same configuration there is no issue in transmit. Also in receive if I send less than 10 bytes then it's working without an issue but if number of bytes increase RX interrupt stopped.Then I configured LPUART baudrate 9600 and in this case everything working as expected.So, Can you please let me know that LPUART can be work on 57600 baudrate or not?Also please share the configuration to make it work on 57600 baudrate. Thanks.
I have a custom pcb using a Seeed WIO-E5 module. I found a github repo that supports the WIO-E5. After downloading it and loading it onto my custom pcb my node joins the network and seems to work. I notice however that the setting in the .ioc file shows Can someone tell me if I should change this given I have a custom PCB?I then go in to adjust pinout to reflect my pcb and have found that changing io pins in the ioc makes the end node very susceptible to not wanting to join the network. I have not had much luck wrt adapting this firmware so as a follow up question:I have NOT found a good library or examples that support the STM32WLE5 (single core) anywhere on STMicro site. Can someone please tell me how to start from a blank STM32WLE5 as an end node? Are there libraries somewhere for this chip to download? (I see a ton of support for the STM32WL55 (dual core) but virtually nothing for the single core and SEEED only supports the custom FW t
Hi all.I have been working with STM32WB for over a year and now starting up to use zigbee.Been trying the examples and digging deep into the internet on how to send values from a STM32WB that acts an temperature sensor. Not much info on ST & zigbee.I can make it show up in the coordinator, but I have not been able to register it as a temperature sensor and send values.Most of the examples show how to handle OnOff toggle, and its not really clear on how to set it up to send values.Also to set up multiple values to be able to send multiple sensor types.If anyone have an example or just like to copy a few lines of how you did it, would help tremendous.Many big thanks beforehand // Mike
Hi , I am working with STM32WB55RG-NUCLEO board. I've managed to upload the BLE_Stack_Full_FW and then when I try the example codes for BLE on my board, I can see the BLE advertising on my ST BLE ToolBox.However, when I try to follow the ST's youtube videos and other tutorials for creating a new project by hand, I follow these steps below:Create a project for STM32WB55RG-NUCLEO board with or without the default settings and open IOC file.System Core -> Activate HSEMSystem Core -> Activate IPCC (with both interrupts active)System Core -> RCC -> HSE & LSE set to "Crystal/Ceramic Res."Timers -> RTC -> Activate Clock Source and set WakeUp to "Internal WakeUp" (with interrupt active)Connectivity -> RF -> Activate RF1Middleware and Software Packs -> STM32_WPAN -> Activate BLESTM32_WPAN -> BLE Applications and Services -> Custom Template enabled, others are disabledSTM32_WPAN -> BLE Advertising -> Include AD_TYPE_COMPLETE_LOCAL_NAME_ELEMENT
Hi all,The STM32WLE MCU's wireless part features two output pins, one for high power and another for low power.In the schematic diagram, both of these pins are linked to inductors: RFO_LP connects to L10, and RFO_HP connects to L9.It's worth noting that in the L9 position on the schematic, there is a 0-ohm resistor.After reviewing alternative schematic versions, such as the lowband variant, I observed that both pins are associated with inductors, but their part numbers correspond to 0-ohm resistors.Can someone clarify whether L9 should contain an inductor or a resistor, and if it's an inductor, what should its nominal value be?
I have successfully configuration P-NULCEO-WB55 as central(beacon observer) device using \STM32Cube_FW_WB_V1.4.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_p2pClient example. ACI_GAP_START_GENERAL_DISCOVERY_PROC event ends after 10 seconds. Is there any way to reduce this 10 seconds time?
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.