Skip to main content
Slh
Senior
Nov 6, 2023 2:35 PM UTC
Question

WIFI Support on STM32W?

Sometimes, if in addition to Bluetooth, WIFI is needed in the development of a product, the third module is used. Does ST plan to include WIFI in the e.g STM32W series in the future?

This topic has been closed for replies.

3 replies

STTwo-32
ST Technical Moderator
Nov 6, 2023 3:18 PM UTC

Hello @Slh and welcome to the ST Community :smiling_face_with_smiling_eyes:.

At the moment, we don't have such a series. If you are looking for an ST Board that give you the opportunity to work with both Wi-Fi and Bluetooth. I suggest you use the B-U585I-IOT02A Discovery kit wish would provide Wi-Fi and Bluetooth communication and other interfaces that may help you.

Best Regards.

STTwo-32.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Piranha
Principal III
Nov 7, 2023 2:46 AM UTC

The author specifically asked about an integrated Wi-Fi, not a separate 3rd party module. Yet you are recommending exactly a 3rd party module. The real answer, which you should have given, is:

  1. There currently is no such a device in STM32 series.
  2. Tell whether such a device is considered and/or planned, if you can share such information.