Skip to main content
Associate
Oct 31, 2023 12:29 PM UTC
Solved

Nucleo-WB15CC : Can't erase all flash sectors

Hi, I am working with a NUCLEO-WB15CC and can't erase all of the 320 KBytes Flash. When using the STM32_Programmer_CLI the following works perfectly fine:

STM32_Programmer_CLI.exe -c port=SWD -e [0 55]

but with

STM32_Programmer_CLI.exe -c port=SWD -e [0 56]

or any other value larger than 55 of the upper sector index, I get the error message

Error: Sector erase operation failed at least for one of the existing specified sectors

I already tried to reset the board to factory settings (as proposed in other posts) by

STM32_Programmer_CLI.exe -c port=SWD reset=HWrst -w32 0x5800040c 0x00008000

This didn't help and I'm running out of ideas. Any suggestions? Thanks in advance.

--

Enclosed is the output of the command to display the option bytes by

STM32_Programmer_CLI.exe -c port=SWD -ob displ

-------------------------------------------------------------------
STM32CubeProgrammer v2.12.0
-------------------------------------------------------------------

ST-LINK SN : 066EFF363946433043082412
ST-LINK FW : V2J37M27
Board : NUCLEO-WB15CC
Voltage : 3.28V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x494
Revision ID : Rev Z
Device name : STM32WB1xxx
Flash size : 320 KBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xB1

UPLOADING OPTION BYTES DATA ...

Bank : 0x00
Address : 0x58004020
Size : 60 Bytes

Bank : 0x01
Address : 0x5800403c
Size : 4 Bytes

Bank : 0x02
Address : 0x58004080
Size : 8 Bytes

OPTION BYTES BANK: 0

Read Out Protection:

RDP : 0xAA (Level 0, no protection)

BOR Level:

BOR_LEV : 0x0 (BOR Level 0 reset level threshold is around 1.7 V)

User Configuration:

nBOOT0 : 0x1 (nBOOT0=1)
nBOOT1 : 0x1 (Boot from code area if BOOT0=0 otherwise system Flash)
nSWBOOT0 : 0x0 (BOOT0 taken from the option bit nBOOT0)
SRAM2RST : 0x1 (SRAM2 is not erased when a system reset occurs)
SRAM2PE : 0x1 (SRAM2 parity check disable)
nRST_STOP : 0x1 (No reset generated when entering the Stop mode)
nRST_STDBY : 0x1 (No reset generated when entering the Standby mode)
nRSTSHDW : 0x1 (No reset generated when entering the Shutdown mode)
WWDGSW : 0x1 (Software window watchdog)
IWDGSTDBY : 0x1 (Independent watchdog counter running in Standby mode)
IWDGSTOP : 0x1 (Independent watchdog counter running in Stop mode)
IWDGSW : 0x1 (Software independent watchdog)
GPIO_MODE_PB11: 0x1 (If RESET_MODE_PB11 = 0: Standard GPIO pad functionality, Only internal RESET possible. If RESET_MODE_PB11 = 1: Bidirectional reset, NRST pin configured in reset input/output mode (default mode), GPIO functionality is not available on PB11.)
RESET_MODE_PB11: 0x1 (If GPIO_MODE_PB11 = 0: Reset input only, a low level on the NRST pin generates system reset, internal RESET not propagated to the NSRT pin. If GPIO_MODE_PB11 = 1: Bidirectional reset, NRST pin configured in reset input/output mode (default mode).)
IRH : 0x1 (Internal resets drives NRST pin low until it is seen as low level.)

ESE:

ESE : 0x1 (Security enabled)

PCROP Protection:

PCROP1A_STRT : 0x1FF (0x807FC00)
PCROP1A_END : 0x0 (0x8000400)
PCROP_RDP : 0x0 (PCROP zone is kept when RDP is decreased)
PCROP1B_STRT : 0x1FF (0x807FC00)
PCROP1B_END : 0x0 (0x8000400)

Write Protection:

WRP1A_STRT : 0xFF (0x807F800)
WRP1A_END : 0x0 (0x8000000)
WRP1B_STRT : 0xFF (0x807F800)
WRP1B_END : 0x0 (0x8000000)
OPTION BYTES BANK: 1

IPCCDBA-AA:

IPCCDBA : 0x0 (0x20010000)
OPTION BYTES BANK: 2

Security Configuration Option bytes:

SFSA : 0x38 (0x801C000)
FSD : 0x0 (System and Flash secure)
DDS : 0x1 (CPU2 debug access disabled)
C2OPT : 0x1 (SBRV will address Flash)
BRSD_B : 0x0 (SRAM2b is secure)
SBRSA_B : 0x0 (0x20038000)
BRSD_A : 0x0 (SRAM2a is secure)
SBRSA_A : 0xA (0x20032800)
SBRV : 0x11800 (0x8000000)

 

This topic has been closed for replies.
hbtestBest answer
Associate
Nov 7, 2023 1:57 PM UTC

Ok, obviously SFSA is set to 0x38 (0x801C000), which translates to 56 pages of 2 KB and 112 KB in total, and in the Release Notes for STM32WB Copro Wireless Binaries it is written "The SFSA option byte can only be set by the CPU2. The user cannot modify that value.". This explains the behavior and we have to live with this restriction.

Reading the documentation can sometimes be quite helpful. :smiling_face_with_smiling_eyes:

1 reply

hbtestAuthorBest answer
Associate
Nov 7, 2023 1:57 PM UTC

Ok, obviously SFSA is set to 0x38 (0x801C000), which translates to 56 pages of 2 KB and 112 KB in total, and in the Release Notes for STM32WB Copro Wireless Binaries it is written "The SFSA option byte can only be set by the CPU2. The user cannot modify that value.". This explains the behavior and we have to live with this restriction.

Reading the documentation can sometimes be quite helpful. :smiling_face_with_smiling_eyes: