Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
I'm developing an end-node based on the STM32 Nucleo-L476RG with a LoRa module SX1272MB2DAS and a Grove sensor (based on DHT11). I'm facing a dilemma regarding how to retrieve data from the sensor. I'm torn between two options: modifying the data retrieval method in the I-Cube-Lrwan example (rather than using I2C) or implementing my own middleware in a new project. Which approach would you recommend, and how could I effectively implement it?
We are developing a BLE device based on a STM32WB5MM. The device acts as a server and has configured the connection with bonding (and a passkey).We have a problem connecting to the device when several devices of the same type coexist in the same place (about 3/4 devices in an area of 5 meters radius). It is difficult to start the connection, in the order of minutes (sometimes it is not even possible to start the connection). However, once the connection is established (because we move away from the area) it remains stable (even if we return to the area with more devices).Any idea why this might be? All devices have the same name. This is the only thing that comes to mind. Can this cause a problem at the time of authentication (bonding)? We have noticed that if a mobile device (which is our client) has a paired device, it cannot connect/pair to another one until the information of the previous device has been deleted on the mobile. If so, just modifying the name of the advertising is en
I also found programming by serial line in below using STM32F446. Does STM32 has a 'naming convention' for timer, (Like, Basic, Enhanced, etc....), such that I can 'quickly' see if the timer inside our STM32WLE5JC target MCU will have the 'link/slave' capability as the example STM32F446. https://community.st.com/t5/stm32-mcus-products/generate-fixed-number-of-pulses-in-stm32f446me/m-p/216485 an4776-generalpurpose-timer-cookbook-for-stm32-microcontrollers-stmicroelectronics --- [you can find the original thread, from which this one was split off, here]
ACI_L2CAP_CONNECTION_UPDATE_RESP_EVENTWhat is the Result field? Need to know if change accepted
Dear All,I am search for an example BLE beacon code for the NUCLEO-WB55RG board which solely uses the HCI layer.There is an example for the WBA board: https://github.com/STMicroelectronics/STM32CubeWBA/tree/main/Projects/NUCLEO-WBA55CG/Applications/BLE/BLE_BeaconHCI Is there somewhere an analog example code for the NUCLEO-WB55RG board available?Or does this code also work for the mentioned board? Thanks in advise. Regards,Andreas
I am trying to enable all 3 UARTS (LPUART, USART1 and USART2) within the STM IDE. However, on choosing LPUART, USARTS2 become unavailable (and vice versa) . Is this a device limitation? We really would like to be able to use all 3 uarts (no flow control necessary)
Hi, I would like to disable/re-enable BLE and keep the concurrent Zigbee stack in normal operation. Some other posts suggested to call hci_reset() to disable BLE and re-initialize it later when needed again.After calling hci_reset() somehow Zigbee wont join the network anymore.Are there shared components between the hci and Zigbee? Is what I am trying to achieve even possible with the tm32wb5x_BLE_Zigbee_FFD_dynamic_fw stack (I am using a P-NUCLEO-WB55)?Thank you for any hint! Best Regards,Alexander
Hello all,I have purchased the p-nucleo-lrwan2 set that has a gateway and a end node. In the tools and software they have mentioned how to connect the gateway with LORIOT,TTN and Acitility. But I have a requirement such that gateway and end node-1 (i-nucleo-lrwan from the kit), end node-2(sx1276mb1mas shield with nucleo-l466rg) has to be connected to AWS and establish communication with each other. https://www.st.com/en/evaluation-tools/p-nucleo-lrwan2.html#overviewLooking forward for the support. Thanks in advance.
How STM32WLE5JC pin PAD circuit works in mixed 3 volts Vdd and 4.2 volts for Open Drain Output pin? Would like to switch medium power LED that takes 45mA and supplied directly by 4.2 volts Li ion cell. LDO, MCP1700, drops cell voltage from 4.2 to 3V to feed MCU four power pins.Use 3 port pins and each sink 15mA. Configure pin as Open Drain, disable pull up. Disable pull down. Use PA4, PA5 and PA6 that have I/O structure type FT. Is it correct that PA4, PA5 and PA6 can take 3 + 3.9 = 6.9 volts and it is OK in this circuit that put 4.2 volts on IO pin when LED is off? TIA
I have found :C:\STM32WL_WS\Hands-on\Point2Point_Phy\Projects\NUCLEO-WL55JC\Applications\SubGHz_Phyand also :C:\STM32Cube_FW_WL_V1.3.0\Projects\NUCLEO-WL55JC\Applications\SubGHz_Phy\SubGHz_Phy_PingPongBut it is very difficult to work on this ... by example ..it is impossible to do "copy and paste".... Thank you in advance...!! Daniel Julio Abaddanieljabad@yahoo.it
HI,All I noticed that when we use BLE stack, we must set SYSCLK to 16MHz。When i set the SYSCLK upto 100MHz,the uart1 log will be garbled after call BleStack_Init which contained in st ble stack lib。I don't know if my discovery is correct。I don't understand why ST doesn't provide the source code for the Bluetooth protocol stack。
Is the STM32CubeIDE defaults 64 bits in unix time? if not, how/where to put gcc command line option in STM32CubeIDE "gcc -D_TIME_BITS=64". Supposedly, this will redirect unix time to be 64 bit instead of traditional 32 bit that will overflow in year 2038. TIA
Would appreciate pointer and insignt on learning how to do battery minimum energy LoRa on (a) half a dozen of sleep modes (b) example sequencer C coding with power saving (c) reading list on application/tech notes, etc. TIA
HelloIs there any RF layout documentation for STM32WB1MMC? Minimum ground plane size, distance to PCB edges, copper clearance etc? I can't find anything.Thanks
I received my first STM32WB5MM-DK.Reeded AN5289 first 104 pages to understand the architecture of the examples.And watched this youtube playlist "STM32WB Getting Started Series". So after importing the Heart Rate example with cubeIDE (Version: 1.14.1) it worked, but after re-generating the code via cube the code cant compile.I even tried to start from scratch and set the IOC (uploaded to this post) with STM32_WPAN (rf, rtc, sys...), all compiled but no advertise received via phone app.Used with: STM32CubeWB Firmware Package V1.18.0 Uploaded the IOC, if support can please check out the configuration and find what is wrong.Or, There is updated guide to use the latest platform?
Hi,I am making Zigbee based project and I tried to use the P-Nucleo-WB55 and using STM32CubeIDE v1.15. Once I downloaded the CubeWB1.19 and compiled the Zigbee apps but none of those apps working. It always shows the Fatal Error saying Unknown, when I check the code it is checking the FW version and it is not in there so it stops. Is there any solution to resolve this issue? thanks,YJ
I am using an STM32WB5MMG for a BLE application. The device acts as a server. I have configured a number of characteristics with indication permissions. How can I confirm the correct reception of the characteristics updates by the client? I mean, where can I get the indication confirmation?Best regards and thanks.
Hi this is not a specific Stm32WB question, but still relevant for any BLE development.I am working on a STM32WB design. I wanted to see what happens when I have different Bluetooth chips on the host side. SO I bought a TP-LINK bluetooth USB dongle. As soon as I attached this USB dongle to my laptop, no usb isn working on my laptop anymore. So now bluetooth is not working on my laptop anymore. I cant connect to my old Bluetooth loudspeaker and and and. My ble mouse is still working.what I did so far for recovery:restart laptopremove alle the paired devicesuninstall the device driver in device manager and restarttry a different USB Bluetooth dongle.Any further ideas?
Hello community,I'm trying to create a Lora node with a STM32L4 board and a SX1272 transceiver. I am quite new to Lora and I don't see how to connect them (I have a XBee adp V1.0 for interface).Does someone have any clue about how can I make it work ?Also i found that STM32 boards work with Arduino IDE, but didn't find the example code for the first try of the connectionThanks a lot !
For battery and small size system, STM32WLE5JC is next to a "patch antenna GNSS module", how you think about two choices?1. Use low MCU clock frequency. MCU active for LONGER time, then finish the work and go to STOP2 with RTC on. I believe low MCU freq is less noisy (but noise duration is longer), right?2. Use high MCU freq. MCU active for SHORTER time and then STOP2 with RTC on. I believe high freq is more noise (but noise duration is shorter), right?TIA
I would like to write C code for the above board. From reading, I believe the steps are as follow. Appreciate if you may help to see if any issue. TIA1. I have Nucleo F103RB (and also F401RE) to be used as ST LINK programmer2. I did firmware upgrade to Nucleo F103 and it is now ST-LINK V2 FW : V2J42M27 Debug + VCP. It will work right? Although the Nucleo WL5JC board has ST Link V4.3. I plug in the Nucleo F401 and hit the "update firmware" buttom. Current firmware is V2J43M28. It suggests to "update" to V2J42M27 Debug + mass storage + VCP. Strange the suggest upgrade is one number *LOWER* ? The Nucleo F103 also suggests upgrade to one number LOWER and I did it. I have not yet change the Nueclo F401.3. From UM1724, user manual of Nueclo F103, Remove two jumpers on CN2 connector. CN4 will become six-pin SWD to be connected to the STM32WL5JC target board.4. Does pin 1 on Nueclo F103 and F401 outputs 3.3 volts to power the ta
Is there a new "standard" way to handle time other than the original UNIX time was mentioned in AN5406 - Rev 7 - How to build a LoRa® application with STM32CubeWL, which will overflow in year 2038?TIA
Hi,I´m just starting with Matter over Thread (with the Lighting-App from github).I´m a little bit confused which binary is for which purpose, because the file various file names:- BLE_Thread_dynamic / static (from STM32Cube_FW_WB_V1.19.0)- Thread_xxx (from STM32Cube_FW_WB_V1.19.0)- BLE_Thread_ForMatter (from the github example) Especially for me the difference between Thead and Thread for Matter is not clear.Which is the right one for the Github Lighting example?Best regards, Achim
Is the source code used to generate the Wireless binaries for STM32WB55 co-processor accessible?I am looking for the source code of stm32wb5x_BLE_xxxxx.bin.Regards,Bastien
Is STM32CubeWL the current HAL for use with STM32WL5JC Lora MCU? version 1.3.0 https://www.st.com/en/embedded-software/stm32cubewl.htmlIs the STM32Cube_FW_WL outdated and replaced by the above?TIA
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.