Skip to main content
Associate III
Apr 16, 2024 9:09 PM UTC
Solved

Optimal MCU clock frequency to reduce EMI interference to co-exist GNSS receiver

For battery and small size system, STM32WLE5JC is next to a "patch antenna GNSS module", how you think about two choices?

1. Use low MCU clock frequency.  MCU active for LONGER time, then finish the work and go to STOP2 with RTC on.  I believe low MCU freq is less noisy (but noise duration is longer), right?

2. Use high MCU freq.  MCU active for SHORTER time and then STOP2 with RTC on.  I believe high freq is more noise (but noise duration is shorter), right?

TIA

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Apr 24, 2024 2:20 PM UTC

Hello @David_ 

For More data about GNSS, look at our GNSS Positioning Forum where you may find more help.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

5 replies

Tesla DeLorean
Guru
Apr 16, 2024 9:28 PM UTC

Put the GNSS antenna on the opposite side of the board to ALL the active electronics. 

Shield it the receiver and RF path

The Intermediate Frequencies in the front-end are typically quite low, in the couple of MHz range. GPS Gold Codes are at 1.023 MHz +/- 3 KHz depending on the motion/doppler and local clock bias.

Some receivers have spectrum analyzer modes, so you can see the in-band interference.

I'd probably favour doing stuff quickly, and limiting radio transmit time.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
David_Author
Associate III
Apr 16, 2024 9:56 PM UTC

Many thanks.  Any idea which brand/model of single frequency standard precision GNSS receiver (the better unit of this grade with stimutanelous five constellations) has spectrum analyzer modes?  OR, it is domain of survey grade receiver?  TIA

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Apr 24, 2024 2:20 PM UTC

Hello @David_ 

For More data about GNSS, look at our GNSS Positioning Forum where you may find more help.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.