Question
Wireless Copro binaries
Hi,
I´m just starting with Matter over Thread (with the Lighting-App from github).
I´m a little bit confused which binary is for which purpose, because the file various file names:
- BLE_Thread_dynamic / static (from STM32Cube_FW_WB_V1.19.0)
- Thread_xxx (from STM32Cube_FW_WB_V1.19.0)
- BLE_Thread_ForMatter (from the github example)
Especially for me the difference between Thead and Thread for Matter is not clear.
Which is the right one for the Github Lighting example?
Best regards,
Achim