Question
STM32cubeide linux WSLg under windows10
I've tried using WSLg into windows 10 to start a project using the STM32cubeide but it fails. The ide is launched but those not automaticaly download stuff, but manualy do. If click new project, target selector animation goes and then I have this message "STM32 target or STM32Cube example selection is required". So can't select mpu. etc...
What is the simplest way to start dev :
- full linux machine
- virtual machine
- WSLg /w10 should work
Thx for any help.