2021-03-10 03:07 PM
Hello
I use STM32CubeProg 1.6 to configure my stm32wb55. If I use ST-Link there are two bookmarks and if I use USB boot there is only one bookmark. Is it ok?
And also there are a lot of error while I try to set option bytes via ST_Link.
P.S. Please make CubeProg GUI a part of CubeIDE.
@Imen DAHMEN
2021-03-18 09:33 AM
Hi @dungeonlords789 ,
If your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Houda
2021-03-18 09:39 AM
Thank you
1) "or difference between Debug and Bootloader option bytes display , it's coming from a tool internal implementation detail which doesn't impact the final user.If you are facing any issue with that I can report it to Development team." I think it is not ok that in boot mode I see one set of bookmarks and in debug mode I see another set...
2) ok, in my case ESE bit is read only . So CubeProg should say "ESE bit is readonly in debug mode", but CubeProg says "ESE does not exist". It isn't the same.
2021-03-19 01:00 AM
Hi @dungeonlords789 ,
Houda
2021-11-08 08:49 PM