Can't display TouchGFX graphics
- 11 replies
- 4243 views
Hello everyone. I am currently working with an STM32F469I-Discovery Board.
I created my project using the STM32CubeIDE board selector and made my layout using TouchGFX. Both softwares communicate as it should and I can generate code from one software and see the changes in the other one. I successfully added a task to FreeRTOS so I know I can correctly program the board and that it is working. I also tested an example showing me that the screen is working as it should too.
Now comes my problem. I am completely unable to display anything on the screen that has been created using TouchGFX and STM32CubeIDE. I configure the LTDC as well as the DSI in all imaginable configurations and nothing is working.
I was expecting it to be rather straight forward, without barely touching anything:
- create the project in STM32CubeIDE (screen and communication configured by the IDE),
- modify the TouchGFX file to look as I want,
- generate the code,
- built and debug the code in STM32CubeIDE,
- the display shows up.
Do I need to check anything else? I was thinking of maybe a faulty GUI task or something like that. I have attached my code so you may be able to run it on your own STM32F469I-Disco and check if I missed something obvious.