Skip to main content
Wjian.1
Associate III
Oct 23, 2020 9:31 AM UTC
Question

NETDEV WATCHDOG: eth0 (cpsw): transmit queue 0 timed out

Hi:

​Anyone familiar with this issue?When I plug in the network cable, the following information will be printed later:

​

[ 373.607360] ------------[ cut here ]------------

[ 373.610551] WARNING: CPU: 1 PID: 0 at net/sched/sch_generic.c:447 dev_watchdog+0x300/0x304

[ 373.618870] NETDEV WATCHDOG: eth0 (stm32-dwmac): transmit queue 0 timed out

[ 373.625765] Modules linked in: aes_arm_bs crypto_simd cryptd algif_skcipher brcmfmac cfg80211 galcore(OE) hci_uart brcmutil btbcm stm32_cec spi_stm32 sch_fq_codel ipv6 nf_defrag_ipv6

[ 373.642115] CPU: 1 PID: 0 Comm: swapper/1 Tainted: G          OE    5.4.31 #1

[ 373.649368] Hardware name: STM32 (Device Tree Support)

[ 373.654536] [<c01124dc>] (unwind_backtrace) from [<c010d784>] (show_stack+0x10/0x14)

[ 373.662275] [<c010d784>] (show_stack) from [<c0bead54>] (dump_stack+0xb0/0xc4)

[ 373.669510] [<c0bead54>] (dump_stack) from [<c0125b24>] (__warn+0xd0/0xf8)

[ 373.676384] [<c0125b24>] (__warn) from [<c0125f00>] (warn_slowpath_fmt+0x98/0xc4)

[ 373.683872] [<c0125f00>] (warn_slowpath_fmt) from [<c0a9eac4>] (dev_watchdog+0x300/0x304)

[ 373.692063] [<c0a9eac4>] (dev_watchdog) from [<c019ca4c>] (call_timer_fn+0x3c/0x20c)

[ 373.699812] [<c019ca4c>] (call_timer_fn) from [<c019d1ec>] (run_timer_softirq+0x218/0x5d0)

[ 373.708087] [<c019d1ec>] (run_timer_softirq) from [<c01022f0>] (__do_softirq+0x148/0x43c)

[ 373.716276] [<c01022f0>] (__do_softirq) from [<c012ca8c>] (irq_exit+0xc8/0xe0)

[ 373.723504] [<c012ca8c>] (irq_exit) from [<c017a4b4>] (__handle_domain_irq+0x80/0xe8)

[ 373.731350] [<c017a4b4>] (__handle_domain_irq) from [<c05e2a58>] (gic_handle_irq+0x4c/0x90)

[ 373.739705] [<c05e2a58>] (gic_handle_irq) from [<c0101a8c>] (__irq_svc+0x6c/0xa8)

[ 373.747182] Exception stack(0xdf0c5f80 to 0xdf0c5fc8)

[ 373.752241] 5f80: 00000000 00050fcc dfaf5074 c011b740 00000001 df0c4000 c1204ea8 c1204ee8

[ 373.760428] 5fa0: c000406a 410fc075 00000000 00000000 00000000 df0c5fd0 c010a1a4 c010a1a8

[ 373.768606] 5fc0: 60010013 ffffffff

[ 373.772101] [<c0101a8c>] (__irq_svc) from [<c010a1a8>] (arch_cpu_idle+0x38/0x3c)

[ 373.779503] [<c010a1a8>] (arch_cpu_idle) from [<c0158404>] (do_idle+0xc4/0x14c)

[ 373.786817] [<c0158404>] (do_idle) from [<c0158778>] (cpu_startup_entry+0x18/0x20)

[ 373.794394] [<c0158778>] (cpu_startup_entry) from [<c010268c>] (__enable_mmu+0x0/0x14)

[ 373.802389] ---[ end trace 6e1a18e6e110c983 ]---

Thanks & Regards

This topic has been closed for replies.

6 replies

AgaGioUmpiSrl
Associate II
Oct 28, 2020 5:04 PM UTC

I have a similar problem when I start the firmware on the M4 core ...

[ 224.064973] ------------[ cut here ]------------

[ 224.068178] WARNING: CPU: 0 PID: 0 at net/sched/sch_generic.c:466 dev_watchdog+0x248/0x24c

[ 224.076364] NETDEV WATCHDOG: eth0 (stm32-dwmac): transmit queue 0 timed out

[ 224.083267] Modules linked in: brcmfmac galcore(O) cfg80211 brcmutil

[ 224.089592] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G      O   4.19.94 #1

[ 224.096932] Hardware name: STM32 (Device Tree Support)

[ 224.102069] [<c031269c>] (unwind_backtrace) from [<c030cd3c>] (show_stack+0x10/0x14)

[ 224.109753] [<c030cd3c>] (show_stack) from [<c0ee542c>] (dump_stack+0xb0/0xc4)

[ 224.116934] [<c0ee542c>] (dump_stack) from [<c0347130>] (__warn.part.3+0xbc/0xd8)

[ 224.124370] [<c0347130>] (__warn.part.3) from [<c03471b4>] (warn_slowpath_fmt+0x68/0x8c)

[ 224.132415] [<c03471b4>] (warn_slowpath_fmt) from [<c0db0370>] (dev_watchdog+0x248/0x24c)

[ 224.140552] [<c0db0370>] (dev_watchdog) from [<c03b9508>] (call_timer_fn+0x3c/0x200)

[ 224.148249] [<c03b9508>] (call_timer_fn) from [<c03b98d8>] (expire_timers+0xb4/0x15c)

[ 224.156034] [<c03b98d8>] (expire_timers) from [<c03b9cc4>] (run_timer_softirq+0xac/0x1ac)

[ 224.164168] [<c03b9cc4>] (run_timer_softirq) from [<c0302274>] (__do_softirq+0x14c/0x420)

[ 224.172303] [<c0302274>] (__do_softirq) from [<c034d4c0>] (irq_exit+0xc8/0xdc)

[ 224.179482] [<c034d4c0>] (irq_exit) from [<c039ad44>] (__handle_domain_irq+0x80/0xec)

[ 224.187271] [<c039ad44>] (__handle_domain_irq) from [<c069e528>] (gic_handle_irq+0x58/0x9c)

[ 224.195573] [<c069e528>] (gic_handle_irq) from [<c0301a0c>] (__irq_svc+0x6c/0xa8)

[ 224.203004] Exception stack(0xc1801f10 to 0xc1801f58)

[ 224.208027] 1f00:                   00000000 00026bb0 dbb7d54c c031e220

[ 224.216162] 1f20: ffffe000 c1804c78 c1804cbc 00000001 c1804c48 00000000 c175e628 c13ddc1c

[ 224.224292] 1f40: c1804d58 c1801f60 c0309384 c0309388 60030013 ffffffff

[ 224.230873] [<c0301a0c>] (__irq_svc) from [<c0309388>] (arch_cpu_idle+0x38/0x3c)

[ 224.238228] [<c0309388>] (arch_cpu_idle) from [<c0375904>] (do_idle+0x1dc/0x288)

[ 224.245577] [<c0375904>] (do_idle) from [<c0375c88>] (cpu_startup_entry+0x18/0x1c)

[ 224.253105] [<c0375c88>] (cpu_startup_entry) from [<c1600e20>] (start_kernel+0x45c/0x48c)

[ 224.261256] ---[ end trace a68fd34659c8be43 ]---

[ 224.265882] stm32-dwmac 5800a000.ethernet eth0: Reset adapter.

[ 224.375456] SMSC LAN8710/LAN8720 stmmac-0:00: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=stmmac-0:00, irq=POLL)

[ 225.388528] stm32-dwmac 5800a000.ethernet: Failed to reset the dma

[ 225.393248] stm32-dwmac 5800a000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed

[ 225.402822] stm32-dwmac 5800a000.ethernet eth0: stmmac_open: Hw setup failed

... after that I no longer have the network.

AgaGioUmpiSrl
Associate II
Oct 28, 2020 9:32 PM UTC
PatrickF
ST Employee
Oct 29, 2020 4:00 PM UTC

I confirm that usually error like "Failed to reset the dma" on ETH IP is related to IP does not receive all expected clocks. You should check which https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration is matching your system design.

For detail on ETH clocking, please refer to RCC section in RM0436, look at "Clock distribution for Ethernet (ETH)".

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
ap-swapp
Visitor II
Nov 9, 2020 5:53 PM UTC

ETH clock stops because of incorrect use of SET_BIT macro on rc_w1 registers.

For example this is the case when HAL_SYSCFG_AnalogSwitchConfig() is called.

void HAL_SYSCFG_AnalogSwitchConfig(uint32_t SYSCFG_AnalogSwitch , uint32_t SYSCFG_SwitchState )
 {
  /* Check the parameter */
  assert_param(IS_SYSCFG_ANALOG_SWITCH(SYSCFG_AnalogSwitch));
  assert_param(IS_SYSCFG_SWITCH_STATE(SYSCFG_SwitchState));
  SET_BIT(SYSCFG->PMCCLRR, SYSCFG_AnalogSwitch);
  SET_BIT(SYSCFG->PMCSETR, (uint32_t)(SYSCFG_SwitchState));
 }

The macro SET_BIT is defined as follows:

#define SET_BIT(REG, BIT) ((REG) |= (BIT))

SET_BIT at line 6 of HAL_SYSCFG_AnalogSwitchConfig() function will reset any bit read at logic level 1 (and possibly bits related to ETH clocks that are housed on the same register).

The correct way to manage rc_w1 registers is to write directly the mask containing bits that must be cleared.

The same is true for rs registers.

In the above axample lines 6 and 7 should be:

SYSCFG->PMCCLRR = SYSCFG_AnalogSwitch;
SYSCFG->PMCSETR = (uint32_t)(SYSCFG_SwitchState);

Please note that STM32Cube_FW massively uses SET_BIT macro...

I'm afraid that other registers are wrongly managed in such a way.

Regards.

AgaGioUmpiSrl
Associate II
Nov 9, 2020 6:02 PM UTC

This solves my problem!