Skip to main content
MBert
Associate
December 13, 2019
Question

Break at address "0x1fffca82" with no debug information available

  • December 13, 2019
  • 3 replies
  • 997 views

Hi all...

I'm Matteo from Italy.

I am working with STM32F072 MCU.

Developed my software with STM32F072-EVAL demo board and it works fine (using the on-board STLINK)

Now i am try to debug the same program on my PCB (developed with the same pinout of demoboard) and i getting throubles with debugger (STLINK-V3).

When i press F8 to run the program, i get alwais the Break at address "0x1fffca82" with no debug information available" error.

Just for test I clear the main function as simple as:

HAL_GPIO_WritePin(EXP_OUT1_GPIO_Port, EXP_OUT1_Pin, GPIO_PIN_RESET);
HAL_Delay(10);
HAL_GPIO_WritePin(EXP_OUT1_GPIO_Port, EXP_OUT1_Pin, GPIO_PIN_SET);

well, i found that the error occours in the " HAL_Delay(10); " call.

If I remove the delay function i can debug the set and reset pin (working fine) with step debuf (F6), but when i press F8 i get the same error.

I am using internal HSI48 clock source.

Hereafter the clock configuration:

0690X00000BuaA3QAJ.png

Thank you for help me !

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
December 13, 2019

Running code in the ROM

Make sure BOOT0 pin is held LOW​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MBert
MBertAuthor
Associate
December 13, 2019

Hi Clive!

It works fine!

I am sure i read in some datasheet or application note to leave this pin unconnected :\

Well... Thank you for the advice.

Kind regards!

Ozone
Principal
December 13, 2019

> I am sure i read in some datasheet or application note to leave this pin unconnected :\

Makes sense when a pull-down resistor is connected. Or a pull-up in other cases.

It is usually a favourable habit to check the schematics and the hardware.