cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I am following the Wiki to get started with a STM32MP157C-DK2 but trying to flash I get a segmentation fault error. Error below. I am using a generic micro SD card, as the one supposed to be with the kit was not there. How can I solve this?

AMohr.1
Associate

alex@NUC:~/Projects/stm32mp1/ecosystem/starter-package/stm32mp1-openstlinux-4.19-thud-mp1-19-10-09/images/stm32mp1$ STM32_Programmer_CLI -l usb     -------------------------------------------------------------------

                       STM32CubeProgrammer v2.2.1                 

     -------------------------------------------------------------------

===== DFU Interface  =====

Total number of available STM32 device in DFU mode: 1

 Device Index          : USB1

 USB Bus Number        : 001

 USB Address Number    : 002

 Product ID            : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

 Serial number         : 002900373338510534383330

 Firmware version      : 0x0110

 Device ID             : 0x0500

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @AMohr.1​ 

This is a known issue in V2.2.1. Sorry for inconvenience.

Recommanded version is the V2.2.0.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PatrickF
ST Employee

Alternatively, it should work with v2.2.1 using the GUI instead of command line.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NEW ! Sidekick STM32 AI agent, see here