2019-08-15 10:21 AM
Hello everyone,
I spent the whole day trying to run the software STM32 Cube monitor (version 1.0.3) on my computer.
I have tested with a Linux Mint and a Debian distribution and with the version 11 and 12 of the Oracle Java JDK but the problem is the same.
When I run the software I get the message
Error: Could not find or load main class com.st.mtt.guipower.MainApp
Caused by: java.lang.NoClassDefFoundError: javafx/application/Application
I use the same command of the shortcut to run it
java -jar STM32CubeMonitor-Power.jar
Does anyone know what's the problem? Or if it's possible to download a previous version of the Monitor to test?
Thank you very much for your help.
Solved! Go to Solution.
2019-08-19 12:18 AM
Hello
The tool is working with java 8, the versions 11 and 12 seems not be compatible.
I can see in the user manual : The Java™ SE Run Time Environment 1.8 (version 1.8.121 or newer) from Oracle® must be installed
You should try with a java 1.8 version.
Best regards
Stephane
2019-08-19 12:18 AM
Hello
The tool is working with java 8, the versions 11 and 12 seems not be compatible.
I can see in the user manual : The Java™ SE Run Time Environment 1.8 (version 1.8.121 or newer) from Oracle® must be installed
You should try with a java 1.8 version.
Best regards
Stephane
2019-08-20 3:10 AM
Hi Stephane,
I did as you suggested and it worked with the version 8.
The versions 11 and 12 should also apply to the requirements of the user manual as they are newer, but...
Thank you very much.
Best regards,
Elisio