Skip to main content
MMacn
Associate
Jun 30, 2019 9:54 AM UTC
Solved

CR95HF - error code 0x81

What is explanation for this code (0x81) - can not find it in documentation.

Receiving it for FS2JAST4 chip.

    This topic has been closed for replies.
    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    Jul 1, 2019 9:38 AM UTC

    ​Hi,

    see https://community.st.com/s/profile/0050X0000089G09QAE for similar issue with nRF52.

    Would it be possible to connect a logic analyzer on the SPI link and check the various timings? I suspect something wrong around SPI. Can you also check that the nRF52810 RF part does not cause some noise on the SPI link (i.e. make sure that the RF part is OFF for testing the SPI connection))

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    5 replies

    Brian TIDAL
    ST Technical Moderator
    Jul 1, 2019 8:03 AM UTC

    ​Hi,

    In order to better support you, would you please provide information about your HW and SW setup and about the issue:

    • CR95HF: custom CR95HF board or X-NUCLEO-NFC03A1 or PLUG-CR95HF-B or CR95HF demonstration board
    • MCU: STM32 MCU on Nucleo board or custom board with non ST MCU?
    • Communication interface:
      • SPI or UART
      • configuration: SPI frequency, UART baud rate,
    • SW
      • Linux, RTOS or bare metal application
      • use X-CUBE-NFC3 v2.0.0 library or older X-CUBE-NFC3 library or home made library
    • 0x81 error
      • on which command do you have a 0x81 reply
      • what was the previous command sent to the CR95HF
      • what is the protocol being used and what is its configuration
      • what tag is being used when this issue occurs
      • is it a systematic or a random issue?

    Many thanks

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    MMacn
    MMacnAuthor
    Associate
    Jul 1, 2019 8:35 AM UTC

    Thanks for response =)

    I am using my own pcb with nRF52810 and CR95HF (both from China) - connected via SPI. CR95HF report ID: NFC FS2JAST4

    SW: Segger SAS 4.16 with nRF SDK 15.3

    used commands:

    idncommand[3] = {0x00, 0x01, 0x00};

    setprotocolcommand[5] = {0x00, 0x02, 0x02, 0x01, 0x0F};

    inventorycommand[5] = {0x00, 0x04, 0x02, 0x03, 0x2B};

    readmultiblockcommand[7] = {0x00, 0x04, 0x04, 0x03, 0x23, 0x00, 0x02};

    readblockcommand[6] = {0x00, 0x04, 0x03, 0x03, 0x20, 0x00};

    with different hardware (own pcb Arduino/nRF51 + CR95HF from Mouser) - all works ok.

    tested frequencies from 150k to 2M and modes 0 and 3 - no change in results.

    0x81 response is from various commands - echo, inventory, read block, read multiple block.

    Found:

    when received 0x81 -> re-init SPI, wakeup CR95HF via IRQ, setup SPI, protocol select then repeat command -> no 0x81 - command executed and 0x80 received.

    such behaviour is very frequent - aprox 99% of commands require such re-init procedure to perform correctly. After init/re-init - no more than 2 consecutive commands with 0x00/0x80 response, then 0x81

    I suppose that it can be a "fake CR95HF" case with China IC....

    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    Jul 1, 2019 9:38 AM UTC

    ​Hi,

    see https://community.st.com/s/profile/0050X0000089G09QAE for similar issue with nRF52.

    Would it be possible to connect a logic analyzer on the SPI link and check the various timings? I suspect something wrong around SPI. Can you also check that the nRF52810 RF part does not cause some noise on the SPI link (i.e. make sure that the RF part is OFF for testing the SPI connection))

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Brian TIDAL
    ST Technical Moderator
    Jul 2, 2019 8:19 AM UTC

    Hi,

    I guess you are managing the SPI Slave Select by software. Can you check that the setup time of the Slave Select is inline with the CR95HF datasheet §6.4. You may need to add some delay here.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Brian TIDAL
    ST Technical Moderator
    Jul 4, 2019 4:25 PM UTC

    Hi,

    error 0x81 means Invalid command code. My feeling is that some data are corrupted on the SPI link.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.