cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE and Segger JLink cannot be simultaneously installed! (conflicts with Segger JLink due to udev rules conflict)

GStap
Associate II

If Segger JLink is installed, STM32CubeIDE cannot be installed. See here: https://community.st.com/s/question/0D50X0000AmhtsLSQQ/stmcubeide-installer-failed-on-ubuntu-1804-with-a-dependency-error

If STM32CubeIDE is installed, Segger JLink cannot be installed. See here: https://forum.segger.com/index.php/Thread/6318-Unable-to-install-Segger-JLink-on-Linux-udev-rules-error-possible-conflict-with/#post23198

Please fix this conflict so that we can have *both* installed, as I really would like to work with both. Thank you.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Markus GIRDLAND
ST Employee

There's a ticket for this and I know a colleague of mine has been in contact with Segger to try and work out a solution. I'm uncertain if it will be in the very next release, though.

GStap
Associate II

Thanks for the follow-up! For anyone wondering, meanwhile, a work-around is to simply install STM32CubeIDE and then just add its JLink binaries found in "/opt/st/stm32cubeide_1.0.0/plugins/com.st.stm32cube.ide.mcu.externaltools.jlink.linux64_1.0.0.201904160814/tools/bin" to your PATH environment variable. Now, you can use all JLink executables which are provided by the STM32CubeIDE install right at the command-line like normal. This doesn't allow you to arbitrarily upgrade to any JLink version, but it at least allows you to utilize the ST-provided JLink version that came with the STM32CubeIDE.

See here for details: https://forum.segger.com/index.php/Thread/6318-Unable-to-install-Segger-JLink-on-Linux-udev-rules-error-possible-conflict-with/?postID=23209#post23209