Skip to main content
martonmiklos
Senior
Oct 11, 2018 8:27 AM UTC
Question

STLink V3 host API

In the UM2448 in the 11.5 section the following is present:

The STLINK-V3SET implements an USB interface dedicated to bridge functions from USB

to SPI/I2C/CAN/UART/GPIOs of ST microcontroller target. This interface is firstly used by

STM32CubeProgrammer in order to allow target programming through SPI/I2C/CAN

bootloader.

A host software API is provided in order to extend the use cases.

My questions would be:

  • What kind of host software API is going to be provided? (shared library+headers or something different)
  • What platforms are going to be supported?
    This topic has been closed for replies.

    5 replies

    wan512
    Associate II
    Oct 12, 2018 6:52 AM UTC

    This API should be implemented in {STM32CubeProgrammer}/bin/CubeProgrammer_API.dll.

    ConnectDfuBootloader
    ConnectStLink
    ConnectUsartBootloader
    CubeProgrammerExit
    CubeProgrammerInit
    CubeProgrammerSetDebug
    DeleteInterface
    DeleteLoaders
    DownloadFile
    Execute
    FileOpen
    FreeFileData
    GetDeviceGeneralInf
    GetDfuDeviceList
    GetStLinkList
    GetStorageStructure
    GetUsartList
    InitOptionBytesInterface
    MassErase
    ReadMemory
    ReadUnprotect
    SectorErase
    SetSkipErase
    SwitchOptionBytesConfig
    WriteMemory
    WriteOptionBytes
    checkDeviceConnection
    getCancelPointer
    getExternalLoaders
    getTargetInterfaceType
    removeExternalLoader
    setDisplayCallbacks
    setExternalLoaderPath
    setLoadersPath

    how about wrap them in python/js module officially?

    martonmiklos
    Senior
    Oct 12, 2018 7:40 AM UTC

    @wan512​ 

    Well I am more curious about the I2C, SPI, CAN features.

    They seems to be accessible from the same library at some level:

    SPIInterface::isSecureBL()
    SPIInterface::SendAddress(unsigned int)
    SPIInterface::SPIInterface(int)
    Brg::GetSPIbaudratePrescal(unsigned int, Brg_SpiBaudrateT*, unsigned int*)
    SPIInterface::read32(unsigned int, char*, unsigned int)
    SPIInterface::SPIInterface(int)
    Brg::SetSPIpinCS(Brg_SpiNssLevelT)
    SPIInterface::synchronize()
    SPIInterface::isUBoot()
    SPIInterface::displayConnectParam()
    SPIInterface::ReadUnprotect()
    SPIInterface::readData(unsigned int, unsigned char, int, FileData**, bool)
    SPIInterface::GetCertificate(FileData**)
    SPIInterface::getError(Brg_StatusT)
    SPIInterface::receiveACK(int)
    ConnectSPIBootloader
    SPIInterface::sendByte(unsigned char)
    SPIInterface::erase(unsigned short, unsigned short*)
    SPIInterface::sendData(unsigned char*, unsigned short, unsigned short*)
    SPIInterface::getRDPlevel()
    SPIInterface::receiveAck(int)
    SPIInterface::readBuffer(unsigned int, int, unsigned char*)
    typeinfo for SPIInterface
    SPIInterface::connect(QString)
    SPIInterface::GetDeviceID()
    SPIInterface::getAPnbr()
    SPIInterface::readSspPartition(FileData**)
    SPIInterface::sendBuffer(QByteArray)
    SPIInterface::getPhase()
    SPIInterface::reconnect()
    Brg::WriteSPI(unsigned char*, unsigned short, unsigned short*)
    SPIInterface::getDeviceID(unsigned short*)
    vtable for SPIInterface
    SPIInterface::displayDeviceInfo()
    SPIInterface::programBuffer(unsigned int, char*, unsigned int, TargetMemory)
    SPIInterface::sendSpecialCMD(unsigned char, unsigned short)
    SPIInterface::read16(unsigned int, char*, unsigned int)
    Brg::ReadSPI(unsigned char*, unsigned short, unsigned short*)
    typeinfo name for SPIInterface
    SPIInterface::receiveData(unsigned char*, unsigned int)
    SPIInterface::ReconnectAfterReset(QString)
    SPIInterface::~SPIInterface()
    SPIInterface::start(unsigned int)
    SPIInterface::read8(unsigned int, char*, unsigned int)
    SPIInterface::checkRDPlevel()
    SPIInterface::getDebugInterfaceInfo()
    Brg::InitSPI(Brg_SpiInitT*)
    SPIInterface::~SPIInterface()
    SPIInterface::~SPIInterface()
    SPIInterface::disconnect()
    SPIInterface::getBLversion(unsigned char*)

    The library itself seems to be written in C++ with Qt. Based on the available symbol names it might be possible to came up with an interface, but if it will be officially published that would be the best.

    martonmiklos
    Senior
    Nov 14, 2018 9:19 AM UTC

    FIY: ST mentioned December for the awaited libraries on their blog:

    https://blog.st.com/stlink-v3set-in-circuit-debugger-programmer/

    Similarly, the in-circuit debugger/programmer opens the door to an entirely new set of features as it allows PC developers to drive a couple of GPIOs from the new ST-LINK thanks to the DLLs that are planned for release in December. A

    Markus Rudolf
    Associate III
    Apr 16, 2019 8:46 PM UTC

    Unfortunately they didn't mention which year in December.... Any news on that one?

    Markus Rudolf
    Associate III
    Apr 16, 2019 8:50 PM UTC

    Nevermind, just saw the API folder in the new cube programmer. There is even example programs for visual studio.